This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于HDMI输出延时问题



我们在使用capture然后HDMI显示,发现有大概100ms的延时,中间只是加了个dup和dei然后到显示,请问有什么好的方式,减少延时肉眼无法观察到,我有个疑问bypass模式需要软件干预吗,从程序里,看需要软件来干预,如果可以不需要,我认为应该很快的。请给我一些建议,谢谢!

  • 下面的链接可以参考一下 :

    http://processors.wiki.ti.com/index.php/Latency_Measurement_on_Capture_Encode_Decode_Display_Demo

    你现在的100ms 是怎么测试出来的 ?

  • 通过握拳,可以明显看出有延时,我注意到bp0和bp1,帧率只有35和29

    30: DISPLAY: HDDAC(BP0) : 35 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!!
    [m3vpss ] 5430: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 1, HDDAC(BP0) 1, DVO2(BP1) 1, SDDAC(SEC1) 1
    [m3vpss ] 5430: SYSTEM : FREE SPACE : System Heap = 1660296 B, Mbx = 10238 msgs)
    [m3vpss ] 5431: SYSTEM : FREE SPACE : SR0 Heap = 1140992 B (1 MB)
    [m3vpss ] 5431: SYSTEM : FREE SPACE : Frame Buffer = 896 B (0 MB)
    [m3vpss ] 5431: SYSTEM : FREE SPACE : Bitstream Buffer = 118144 B (0 MB)
    [m3vpss ] 5432: SYSTEM : FREE SPACE : Tiler Buffer = 0 B (0 MB) - TILER OFF
    [m3vpss ] 5432: DISPLAY: Start in progress !!!
    [m3vpss ] 5501: DISPLAY: Start Done !!!
    [m3vpss ] 5501: DISPLAY: DVO2(BP1) : 29 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!!
    [m3vpss ] 5501: SWMS: Start in Progress !!!

    上面结果,我改变了,Vps_platform.c里video输入的时钟,没降低之前,bp0的帧率在57,bp1的帧率在100+,不能正常显示,所以我怀疑时钟分频的问题。为了提高帧率,我不改这个,只改变到dv02的,要怎么修改,谢谢能给我一些帮助。

    /*set digital PLL*/
    pllClk.outputVenc = VPS_SYSTEM_VPLL_OUTPUT_VENC_D;
    pllClk.outputClk = 148500u;//297000u mdf by lqk

    retVal |= Vps_platformControl(
    &gPlatformCommonObj,
    IOCTL_VPS_VID_SYSTEM_SET_VIDEO_PLL,
    &pllClk,
    NULL);

  • 你好;

             如果是 100ms 的延时,通过握拳是感觉不出来的,建议通过 秒表 进行测试延时, 你现在是想hdmi输出到60帧,降低延时 ?