This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678的phy芯片无法配置的问题



您好,

         我们在自制的板子上调试网口,但是link失败,之前在论坛上问需要配置phy芯片。我们硬件配置phy芯片(88e1111)的时候对应的config0和1管脚为000,000,对应phy的地址就是00000。然后又把config4和5配置为111,101。这样对应的hwcfgmode为1111,把接口设置为了gmii。但是phy和6678连接口应该是sgmii。我想通过keystone mdio phy set reg来配置phy,把hwcfgmode改为sgmii,但是现在发现程序卡在了等待写完成的语句上,好像根本没法配phy,这是为啥,请各位大神指教,谢谢!下面是我配置phy的代码。