This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127无法通过串口boot



问题描述:

1、DM8127由于没有接SD口,所以通过串口进行引导,讲DMPC[4..0]配置为00011,上电后,串口终端没有打印“”CCCCC”字符串,串口波特率终端设置为115200

2、使用示波器打DMPC[4]管脚,发现上电后迅速变成高电平,但是该管脚已经使用10K电阻下拉到地,不知为什么会上电后为高电平

3、测量板上各电压、时钟都是正确的。