This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678启动的问题



请问官网的C6678 EVM板子用IBL启动,顺序应该是配置好薄码开关从nand启动后,上电,程序先从IIC加载程序,然后到NAND加载程序,完成启动。可是我现在将DSP和FPGA的CS1或SPI中的时钟线,数据线任意断开一根,就启动不了。串口完全没有任何信息输出。请问是什么原因?

  • 不明白您为什么要去断开这些信号线,FPGA对EVM上的boot,reset,power sequence,clock都是总控的,可能你断开对这些信号造成了影响,进而整版不能工作。您可以仔细看看  《TMDXEVM6678L EVM Technical Reference Manual》 FPGA章节,上面有详细描述的

  • 我现在遇到一个问题,我要使用CS1的SPI来操作一个外设,可是官方的CS1用来和FPGA连接了;于是我就断开DSP和FPGA断开CLK,因为时钟是通过芯片分出来单独给FPGA的,只断开这个,就是简单的断开了和FPGA的联系,可是,发现不能用IBL从Nand Flash启动了,现象是薄码开关打到nand0启动,串口不输出任何信息,我恢复那个clk的串联电阻,就可以启动。我不了解启动会什么会和SPI有什么关系?请指导