This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66ak2h14 dsp电源管理



我现在在使用evmk2h开发板,运行MCSDK(3_00_03_15)中带的uboot,并且debug_options参数设置为1,这样在uboot运行时,仿真器可以调试DSP。查找到uboot下有一个“ psc ”命令控制module的开关(函数名字叫do_psc_cmd),我首先执行“psc  15   di ”  命令关闭DSP CORE0的module,15 是 DSP CORE0的对应序号,指令执行完成后,仿真器确实无法连接DSP0了,但是当我执行"psc  15   en "使能DSP_CORE0时,仿真器仍然无法连接DSP,也就是说一旦module禁能了,使能后也没有效果,请问这是什么原因呢?求解答