hi,
我移植了一个FatFs R0.13版本的到StarterWare软件上,参照官方的Demo。以此来挂载NAND和USB U盘,现在在移植挂载Nand时需要修改FatFs的如下配置
#define FF_MIN_SS 512 #define FF_MAX_SS 512 // NAND: 2048 /* This set of options configures the range of sector size to be supported. (512, / 1024, 2048 or 4096) Always set both 512 for most systems, generic memory card and / harddisk. But a larger value may be required for on-board flash memory and some / type of optical media. When FF_MAX_SS is larger than FF_MIN_SS, FatFs is configured / for variable sector size mode and disk_ioctl() function needs to implement / GET_SECTOR_SIZE command. */
其中根据需求在设置扇区大小为2048来适配Nand的page大小时,发现设置为2048后加载不了U盘,请教一下此种情况是啥问题?