您好,
我最近更換NAND flash,但碰到以下的問題,請問該怎麼解決?謝謝!!
U-Boot 2010.06 (Aug 30 2017 - 15:04:29) DM385_IPNC_3.50.00
NAND device: Manufacturer ID: 0x98, Chip ID: 0xf1 (Toshiba NAND 128MiB 3,3V 8-bit)
NAND read: device 0 offset 0x20000, size 0x1e000
122880 bytes read: OK
U-Boot 2010.06 (Aug 30 2017 - 15:04:50) DM385_IPNC_3.50.00
NAND device: Manufacturer ID: 0x98, Chip ID: 0xf1 (Toshiba NAND 128MiB 3,3V 8-bit)
Data (writethrough) Cache is ON
Loading from NAND 128MiB 3,3V 8-bit, offset 0x280000
Image Name: Linux-2.6.37_CARDVR_3.50.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1763972 Bytes = 1.7 MiB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-2.6.37_CARDVR_3.50.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1763972 Bytes = 1.7 MiB
Load Address: 80008000
Entry Point: 80008000
OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
omap_voltage_late_init: Voltage driver support not added
UBIFS error (pid 1): ubifs_decompress: cannot decompress 2865 bytes, compressor lzo, error -22
UBIFS error (pid 1): read_block: bad data node (block 114, inode 3914)
UBIFS error (pid 1): do_readpage: cannot read page 114 of inode 3914, error -22
UBIFS error (pid 1): ubifs_decompress: cannot decompress 2865 bytes, compressor lzo, error -22
UBIFS error (pid 1): read_block: bad data node (block 114, inode 3914)
UBIFS error (pid 1): do_readpage: cannot read page 114 of inode 3914, error -22
Kernel panic - not syncing: Attempted to kill init!
Backtrace:
[<c0041f70>] (dump_backtrace+0x0/0x110) from [<c02730cc>] (dump_stack+0x18/0x1c)
r6:c6826000 r5:00000007 r4:c0391b58 r3:60000113
[<c02730b4>] (dump_stack+0x0/0x1c) from [<c027312c>] (panic+0x5c/0x178)
[<c02730d0>] (panic+0x0/0x178) from [<c0068858>] (do_exit+0x68/0x5d0)
r3:c0370084 r2:c6829e18 r1:00000001 r0:c030e26b
r7:c682a000
[<c00687f0>] (do_exit+0x0/0x5d0) from [<c0069070>] (do_group_exit+0x84/0xb4)
r7:c682a000
[<c0068fec>] (do_group_exit+0x0/0xb4) from [<c0072f3c>] (get_signal_to_deliver+0x2d0/0x304)
r4:01060013 r3:20000113
[<c0072c6c>] (get_signal_to_deliver+0x0/0x304) from [<c0040f9c>] (do_signal+0x70/0x5f4)
[<c0040f2c>] (do_signal+0x0/0x5f4) from [<c0041ac4>] (do_notify_resume+0x20/0x64)
[<c0041aa4>] (do_notify_resume+0x0/0x64) from [<c003e418>] (work_pending+0x24/0x28)
r4:ffffffff r3:00000000
Best Regards,
Byron