This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x cpsw双网口找不到PHY ID



最近调试AM335x平台网口时,在U-boot下使用mdio接口读写千兆网口dp83867 phy芯片,提示PHY ID跟网口不对应,我们实际硬件连接模式网口0对应的PHY ID = 9,网口1对应PHY ID = 0,内核启动期间根据打印消息提示没检测到PHY ID,设备树的配置及其他调试信息如下截图所示。请高手指点,谢谢!!

硬件设置PHY ID模式如图2所示。

                                                                        图2 u-boot下找不到PHY ID

在u-boot下使用mdio接口读写PHY芯片,提示找不到PHY ID, 硬件配置如图2,3所示。按图2配置模式PHY ID = 9, 图3配置电阻都没焊,PHY ID = 0

                                                     图3  网口0对应PHY芯片配置模式

                                          图4  网口1对应PHY芯片配置模式

内核启动后检测到双网口,如图所示

  • 先检查下上下拉是否是正常的。

  • To Jian Zhou

         检查下第1路上下拉估计是有问题,但奇怪的是目前把第2路PHY 地址(原来是没有配置电阻)配置成跟第1路一样的模式,即PHY地址配置都为9,但内核检测到两个PHY地址分别为4和9,具体如下图1红色标注所示,个人感觉检测顺序有点颠倒,网口0可以正常UP,目前电脑网口配置成100M模式,且跟目标板配置在同一网段,电脑跟目标板用网线直连,仍然ping 不通,具体如图2和3所示。

        问题1:内核检测PHY地址的打印输出的顺序是否跟网口eth0和eth1一一对应??

        问题2:网口eth0 检测到PHY地址,网口eth1没检测到,且网口eth0 显示up,但PC机仍然ping不通目标板

         

                                             图1  内核检测到的PHY 地址

                                                                图2 网口eth0 up

  • 内核开启vlan support,设备树&mac添加duan_emac,注意驱动中寄存器rgmii_sel的设置