你好,现在在设计一个基于AM3352的板子,使用了datasheet中的不带RTC功能的模式,如下图所示:
看里面的意思是当使能RTC内部LDO的时候CAP_RTC是不用接1.1v的,但是查看官网的原理图checklist上,对于这样的应用场景是这样描述的:
现在就是想确认下:在不使用芯片RTC功能的情况,是否还是可以使能内部的RTC-LDO,不用像checklist里面那样还要外接一个1.1v电源?
----------------------------希望尽快回复,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,现在在设计一个基于AM3352的板子,使用了datasheet中的不带RTC功能的模式,如下图所示:
看里面的意思是当使能RTC内部LDO的时候CAP_RTC是不用接1.1v的,但是查看官网的原理图checklist上,对于这样的应用场景是这样描述的:
现在就是想确认下:在不使用芯片RTC功能的情况,是否还是可以使能内部的RTC-LDO,不用像checklist里面那样还要外接一个1.1v电源?
----------------------------希望尽快回复,谢谢。
在不用RTC的情况下,check list里面那个1.1V是必须要连接的。这个往往是要因为要考虑压差带来的漏电流等一系列情况。
所以这里的1.1V并不是为了去使能RTC LDO,就是在RTC disable的时候对于系统的设计。