This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP-TMS320C5505-SPI-clock没有输出信号



Ti工程师您好!

  现在我遇到一个问题,SPI用片选1连接外设AD,但是现在SPI没有输出信号,clock也没有输出信号。
程序是我在例程里修改的,例程里是用SPI往EEPROM里写数据,把例程用ezdsp开发板仿真,也是没有数据的。
不知道哪里出问题了。我下载了好几个版本的例程都不行。








#include <stdio.h>
#include <csl_spi.h>
#include <cslr_spi.h>
#include <csl_sysctrl.h>
#include <csl_general.h>
#include <spirom.h>


#define CSL_TEST_FAILED         (1)
#define CSL_TEST_PASSED         (0)

#define	CSL_SPI_BUF_LEN			(64)
#define	SPI_CLK_DIV				(10000)	
#define	SPI_FRAME_LENGTH		(1)

Uint16 spiWriteBuff[CSL_SPI_BUF_LEN];
Uint16 spiReadBuff[CSL_SPI_BUF_LEN];
Uint16 byteBuf[1];
Uint16 cmdBuffer[3] = {0, 0, 0};

long delay_i;
extern void spirom_write( Uint32 src, Uint16 dst, Uint32 length );
	CSL_SpiHandle	hSpi;

Int16 spi_sample(void)
{
	Int16 			status = CSL_TEST_FAILED;
	Int16 			result;

	SPI_Config		hwConfig;
	Uint16			looper;
	/*Uint16 			value = 0;
	Uint16 			pageNo = 0x0000;
	Uint16			pollStatus;
	Uint16			delay;
	Uint16			fnCnt;*/
	
	result = SPI_init();
    
	if(CSL_SOK != result)
	{
		status = CSL_TEST_FAILED;
		return (status);
	}
	else
	{
		printf ("SPI Instance Intialize successfully\n");
	}

	hSpi = SPI_open(SPI_CS_NUM_1, SPI_POLLING_MODE);

	if(NULL == hSpi)
	{
		return (CSL_TEST_FAILED);
	}
	else
	{
		printf ("SPI Instance Opened successfully\n");
	}

	/** Set the hardware configuration 							*/
	hwConfig.***	= SPI_CLK_DIV;
	hwConfig.wLen		= SPI_WORD_LENGTH_8;
	hwConfig.frLen		= SPI_FRAME_LENGTH;
	hwConfig.wcEnable	= SPI_WORD_IRQ_ENABLE;
	hwConfig.fcEnable	= SPI_FRAME_IRQ_DISABLE;
	hwConfig.csNum		= SPI_CS_NUM_1;
	hwConfig.dataDelay	= SPI_DATA_DLY_1;
	hwConfig.csPol		= SPI_CSP_ACTIVE_LOW;
	hwConfig.clkPol		= SPI_CLKP_LOW_AT_IDLE;
	hwConfig.clkPh		= SPI_CLK_PH_FALL_EDGE;

	result = SPI_config(hSpi, &hwConfig);

	if(CSL_SOK != result)
	{
		return (CSL_TEST_FAILED);
	}
	else
	{
		printf ("SPI Instance Configured successfully\n");
	}

	
	byteBuf[0] = 0xABCD;
	for(looper = 0; looper < 64; )
	{
		spiWriteBuff[looper] = 0x0011;
		spiWriteBuff[(looper + 1)] = 0x00AB;
		spiReadBuff[looper] = 0x0000;
		spiReadBuff[(looper + 1)] = 0x00CD;
		looper += 2;
	}


	return (status);
}


void main(void)
{
	Int16    status;

    pll_sample();                  //时钟初始化
    status = spi_sample();
      
      
      
      
      while(1)
{
	delay_i = 50000;
	while(delay_i--); 
	
    SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);

}	
      
     
}

 
  • 请问用的是哪里的例程?一般我们提供的例程都是在开发板上验证过的。

  •    就是光盘里自带的例程,下边的是例程的全部代码。CSL_SPI_Example_Out  /  csl_spi_example.c

      我用这个程序返回的是:  SPI Sample Test Failed!!!

    /*  ============================================================================
     *   Copyright (c) Texas Instruments Inc 2002, 2003, 2004, 2005, 2008
     *
     *   Use of this software is controlled by the terms and conditions found in the
     *   license agreement under which this software has been supplied.
     *  ============================================================================
     */
    
    /** @file csl_spi_exampale.c
     *
     *  @brief I2S functional layer sample source file
     *
     *  Path: \(CSLPATH)\example\spi\src
     */
    
    /* ============================================================================
     * Revision History
     * ================
     * 09-Sept-2008 Created
     * ============================================================================
     */
    
    #include "csl_spi.h"
    #include <stdio.h>
    
    #define CSL_TEST_FAILED         (1)
    #define CSL_TEST_PASSED         (0)
    
    #define	CSL_SPI_BUF_LEN			(64)
    #define	SPI_CLK_DIV				(8)	
    #define	SPI_FRAME_LENGTH		(1)
    
    Uint16 spiWriteBuff[CSL_SPI_BUF_LEN];
    Uint16 spiReadBuff[CSL_SPI_BUF_LEN];
    Uint16 byteBuf[1];
    Uint16 cmdBuffer[3] = {0, 0, 0};
    
    Int16 spi_sample(void)
    {
    	Int16 			status = CSL_TEST_FAILED;
    	Int16 			result;
    	CSL_SpiHandle	hSpi;
    	SPI_Config		hwConfig;
    	Uint16			looper;
    	Uint16 			value = 0;
    	Uint16 			pageNo = 0x0000;
    	Uint16			pollStatus;
    	Uint16			delay;
    	Uint16			fnCnt;
    	
    	result = SPI_init();
    
    	if(CSL_SOK != result)
    	{
    		status = CSL_TEST_FAILED;
    		return (status);
    	}
    	else
    	{
    		printf ("SPI Instance Intialize successfully\n");
    	}
    
    	hSpi = SPI_open(SPI_CS_NUM_0, SPI_POLLING_MODE);
    
    	if(NULL == hSpi)
    	{
    		return (CSL_TEST_FAILED);
    	}
    	else
    	{
    		printf ("SPI Instance Opened successfully\n");
    	}
    
    	/** Set the hardware configuration 							*/
    	hwConfig.spiClkDiv	= SPI_CLK_DIV;
    	hwConfig.wLen		= SPI_WORD_LENGTH_8;
    	hwConfig.frLen		= SPI_FRAME_LENGTH;
    	hwConfig.wcEnable	= SPI_WORD_IRQ_ENABLE;
    	hwConfig.fcEnable	= SPI_FRAME_IRQ_DISABLE;
    	hwConfig.csNum		= SPI_CS_NUM_0;
    	hwConfig.dataDelay	= SPI_DATA_DLY_0;
    	hwConfig.csPol		= SPI_CSP_ACTIVE_LOW;
    	hwConfig.clkPol		= SPI_CLKP_LOW_AT_IDLE;
    	hwConfig.clkPh		= SPI_CLK_PH_FALL_EDGE;
    
    	result = SPI_config(hSpi, &hwConfig);
    
    	if(CSL_SOK != result)
    	{
    		return (CSL_TEST_FAILED);
    	}
    	else
    	{
    		printf ("SPI Instance Configured successfully\n");
    	}
    	/****************************************************************************/
    	/** This configuration for the EPROM*/
    	 do { /* Check for bsy status */
                value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_BSY);
            }while(value & 0x01==1);
    
    
        CSL_FINS(CSL_SPI_REGS->SPICMD1,SPI_SPICMD1_FLEN,1);       /* set one word */
        /* Send Read Status Command */
        CSL_FINS(CSL_SPI_REGS->SPIDR2,SPI_SPIDR2_DATA,0x0500);
        CSL_FINS(CSL_SPI_REGS->SPIDR1,SPI_SPIDR1_DATA,0x0);
    
        /* set start CMD - Read */
        CSL_FINS(CSL_SPI_REGS->SPICMD2,SPI_SPICMD2_CMD,CSL_SPI_SPICMD2_CMD_READ);
    
        do { /* Check for Word Complete status */
            value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_CC);
        }while(value & 0x02==0);
    
        do { /* Check for bsy status */
            value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_BSY);
        }while(value & 0x01==1);
    
        //Read the Status --- Dummy clock cycles
        CSL_FINS(CSL_SPI_REGS->SPIDR2,SPI_SPIDR2_DATA,0x0);
        CSL_FINS(CSL_SPI_REGS->SPICMD2,SPI_SPICMD2_CMD,0x01);
    
        do { /* Check for Word Complete status */
            value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_CC);
        }while(value & 0x02==0);
        do { /* Check for bsy status */
            value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_BSY);
        }while(value & 0x01==1);
    
        // Enable write using WREN command
        CSL_FINS(CSL_SPI_REGS->SPICMD1,SPI_SPICMD1_FLEN,0x0);
    
        /* Write Enable command */
        CSL_FINS(CSL_SPI_REGS->SPIDR2,SPI_SPIDR2_DATA,0x0600);
        CSL_FINS(CSL_SPI_REGS->SPIDR1,SPI_SPIDR1_DATA,0x0000);
    
        /* set start CMD - Write */
        CSL_FINS(CSL_SPI_REGS->SPICMD2,SPI_SPICMD2_CMD,0x02);
    
        do { /* Check for Word Complete status */
            value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_CC);
        }while(value & 0x02==0);
    
        do { /* Check for bsy status */
            value=CSL_FEXT(CSL_SPI_REGS->SPISTAT1,SPI_SPISTAT1_BSY);
        }while(value & 0x01==1);
    
    	cmdBuffer[0] = 0x02;
        /* eeprom address - MSB */
        cmdBuffer[1] = (pageNo >> 0x08);
        /* eeprom address - LSB */
        cmdBuffer[2] = (pageNo & 0xFF);
    
    	CSL_FINS(CSL_SPI_REGS->SPICMD1,SPI_SPICMD1_FLEN, CSL_SPI_BUF_LEN+3-1);
    	/* Set Command for write */
    	for(fnCnt = 0; fnCnt < 3; fnCnt++)
    	{
    		CSL_SPI_REGS->SPIDR2 = (Uint16)(cmdBuffer[fnCnt] <<0x08);
        	CSL_SPI_REGS->SPIDR1 = 0x0000;
    	
    
    		CSL_SPI_REGS->SPICMD2 = (((CSL_SPI_REGS->SPICMD2) & (Uint16)(~CSL_SPI_SPICMD2_CMD_MASK))
            	            | ((Uint16)(2 << CSL_SPI_SPICMD2_CMD_SHIFT)));
    	
    		do
    		{
    			pollStatus = (CSL_SPI_REGS->SPISTAT1);
    		}while(((pollStatus & 0x02) != 0x01) && ((pollStatus & 0x01) == 0x01));
    	}
    
    	/****************************************************************************/
    	byteBuf[0] = 0xABCD;
    	for(looper = 0; looper < 64; )
    	{
    		spiWriteBuff[looper] = 0x0011;
    		spiWriteBuff[(looper + 1)] = 0x00AB;
    		spiReadBuff[looper] = 0x0000;
    		spiReadBuff[(looper + 1)] = 0x00CD;
    		looper += 2;
    	}
    
    	result = SPI_dataTransaction(hSpi ,spiWriteBuff, CSL_SPI_BUF_LEN, SPI_WRITE);
    	if(CSL_SOK != result)
    	{
    		return (CSL_TEST_FAILED);
    	}
    	else
    	{
    		printf ("SPI Instance Write successfully\n");
    	}
    
    	/******************************************************************************/
    	for (delay = 0; delay < 35000; delay++) {
    		/* no operation */
    	}
    	
       /* Configure the SPI for read from EEprom */
        /* read command */
        cmdBuffer[0] = 0x03;
        /* eeprom address - MSB */
        cmdBuffer[1] = (pageNo >> 0x08);
        /* eeprom address - LSB */
        cmdBuffer[2] = (pageNo & 0xFF);
    
    	CSL_FINS(CSL_SPI_REGS->SPICMD1,SPI_SPICMD1_FLEN, CSL_SPI_BUF_LEN+3-1);
    	/* Set Command for write */
    	for(fnCnt = 0; fnCnt < 3; fnCnt++)
    	{
    		CSL_SPI_REGS->SPIDR2 = (Uint16)(cmdBuffer[fnCnt] <<0x08);
        	CSL_SPI_REGS->SPIDR1 = 0x0000;
    	
    
    		CSL_SPI_REGS->SPICMD2 = (((CSL_SPI_REGS->SPICMD2) & (Uint16)(~CSL_SPI_SPICMD2_CMD_MASK))
            	            | ((Uint16)(2 << CSL_SPI_SPICMD2_CMD_SHIFT)));
    	
    		do
    		{
    			pollStatus = (CSL_SPI_REGS->SPISTAT1);
    		}while(((pollStatus & 0x02) != 0x01) && ((pollStatus & 0x01) == 0x01));
    	}
    	/******************************************************************************/
    	result = SPI_dataTransaction(hSpi ,spiReadBuff, CSL_SPI_BUF_LEN, SPI_READ);
    	if(CSL_SOK != result)
    	{
    		return (CSL_TEST_FAILED);
    	}
    	else
    	{
    		printf ("SPI Instance Read successfully\n");
    	}
    
    	result = SPI_deInit();
    
    	if(CSL_SOK != result)
    	{
    		return (CSL_TEST_FAILED);
    	}
    	else
    	{
    		printf ("SPI Instance deIntialize successfully\n");
    	}
    
    	result = SPI_close(hSpi);
    
    	if(CSL_SOK != result)
    	{
    		return (CSL_TEST_FAILED);
    	}
    	else
    	{
    		printf ("SPI Instance Close successfully\n");
    	}
    
    	
    	for(looper=0; looper < 64; looper++)
        {
            if(spiReadBuff[looper] != spiWriteBuff[looper])
    		{
    			status = CSL_TEST_FAILED;
    			break;
    		}
    		else
    		{
    			status = CSL_TEST_PASSED;
    		}
        }
    
    
    	if(status == CSL_TEST_PASSED)
    	{
    		printf ("SPI Writen & Read buffer matching\n");
    	}
    	return (status);
    }
    
    void main(void)
    {
    	Int16    status;
    
    
    	status = spi_sample();
    
    	if(status != CSL_TEST_PASSED)
    	{
    		printf("SPI Sample Test Failed!!\n");
    	}
    	else
    	{
    		printf("SPI Sample Test Passed!!\n");
    	}
    }
    
  • 跑到是下面到例程么?

    Test Code

    http://support.spectrumdigital.com/boards/usbstk5505/revb/

  • 我之前用SPI的方式将程序拷到eeprom里了,用示波器看是可以看到clock有数据的,但是用例程只是把SPI简单的输出就不行了

  • 是不是EBSR的PPMODE设置不对啊。还有PCGCR1里对SPI的时钟使能。