This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354 RGMII的问题



我们是AM335x+KSZ9031RNX的PHY,是RGMII链接,现在有两个问题:

1.与PC链接的时候自适应经常会识别成百兆

2.自适应成百兆以后,通信一段时间之后,CPDMA就不发送了,DMASTATUS寄存器的TX_HOST_ERR_CODE位是0x0010这个错误,这个错误大概是什么问题,可以这么解决?

  • 追加一个关于RGMII的问题,软件手册上说在RGMII模式下,CONTROL_GMII_SEL寄存器的bit4,5是必须设成1的,因为RGMII不支持内部延迟。但是starterware里面提供的网络样例里面这个寄存器bit4,5上设的是0,两者是矛盾的,请问下哪种是对的?

  • 用的是什么操作系统?Linux吗?

    网络这块,我之前没怎么用过starterware,但是对于LInux来说,确实是有这个delay的配置。而且在代码的部分还会在PHY端通过寄存器的配置,来加入该delay。

    以SDK6.0的uboot代码为例:EZSDK_06_00_00_00/board-support/u-boot-2013.01.01-psp06.00.00.00/board/ti/am335x/board.c

    863 /*
    864 *
    865 * CPSW RGMII Internal Delay Mode is not supported in all PVT
    866 * operating points. So we must set the TX clock delay feature
    867 * in the AR8051 PHY. Since we only support a single ethernet
    868 * device in U-Boot, we only do this for the first instance.
    869 */
    870 #define AR8051_PHY_DEBUG_ADDR_REG 0x1d
    871 #define AR8051_PHY_DEBUG_DATA_REG 0x1e
    872 #define AR8051_DEBUG_RGMII_CLK_DLY_REG 0x5
    873 #define AR8051_RGMII_TX_CLK_DLY 0x100
    874
    875 // if (board_is_evm_sk() || board_is_gp_evm()) {
    876 const char *devname;
    877 devname = miiphy_get_current_dev();
    878
    879 miiphy_write(devname, 0x0, AR8051_PHY_DEBUG_ADDR_REG,
    880 AR8051_DEBUG_RGMII_CLK_DLY_REG);
    881 miiphy_write(devname, 0x0, AR8051_PHY_DEBUG_DATA_REG,
    882 AR8051_RGMII_TX_CLK_DLY);