This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于dsp6678的SGMII调试问题



自己根据开发板设计的板卡,两片DSP,一片phy,一片16端口sgmii switch的bcm5396芯片。 两片dsp的sgmii 0都结在bcm5396上,phy芯片是88e1111,也通过sgmii接到bcm上 phy芯片的配置是 自协商,1000M fullduplex bcm5396不知道怎么配置。 phy芯片和bcm5396均可以单独配置。 现有以下问题: 1.每个dsp都跑完了 ge例程上的internal test都能跑完,现在想测试外部通信,两个 dsp之间通信都需要改什么配置?例程给的说明文件是做的sgmii1口的,看网上说sgmii0例程不支持? 2.在单个dsp上测试ge test serdes loopback时,phy芯片连接rj45到电脑上,电脑通过抓包工具能够收到数据包 这是正常的吗?自己分析是因为连到了bcm上,因为没有配置bcm端口,所以数据包被广播了,因此在pc端能收到! 不知分析的对否? 3.可不可以不用配置5396,让每个dsp之间完成数据收发之后,5396是不是就会自动记住端口呢?