This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320C6747配置SPI0-NOR-FLASH启动,使用128Mbit的FLASH(1.8V外部供电)可以启动,后更换为256Mbit相同封装的SPI-NOR-FLASH(3.3V外部供电),代码不变,不能正常加载启动,使用1.8V供电的FLASH担心不稳定换为3.3V供电的型号,扩为256Mbit后却不能正常启动,需要注意哪些问题让它跑起来呢?谢谢。
3.3v供电的SPI flash电平和C6747的VOH,VOL,VIH,VIL电平匹配么?
另外,可以用仿真器跟踪一下boot过程,看是代码没有加载进来还是加载后没有正确执行?