各位专家:
我们想实现6472与FPGA(V5)通过SRIO进行通信,但是找到的相关资料不多。
想请问下大概流程是怎么样的?DSP应该用哪种模型进行发送(direct IO/message)?
FPGA内部并没有地址这个概念,那LSU寄存器中该如何写地址值呢?
有相关的例程吗?谢谢了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Andy Yin 您好:
初学者还要再麻烦您下:
请问您提到的SRIO例程具体是哪个呢?我看hpdspua和platform_utils_evm6472这两个工程里都没有关于SRIO的文件;在mcsdk_1_00_00_08文件夹里搜索关键字SRIO也没有搜到相应例程。
还有一个问题,我之前没有安装mcsdk时CCS也能识别出6472的6个核,测试DDR,EDMA等驱动时也都正常,现在安装了mcsdk之后我也没有发现有什么区别。那么mcsdk到底是如何发挥作用的呢?
谢谢了!