This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
自己做的SD卡启动分区分了三部分:
mmcblk1boot0 179:8 0 16M 1 disk
mmcblk1boot1 179:16 0 16M 1 disk
mmcblk0 179:24 0 3.7G 0 disk
├─mmcblk0p1 179:25 0 62.8M 0 part
├─mmcblk0p2 179:26 0 1G 0 part
└─mmcblk0p3 179:27 0 2.6G 0 part
mmcblk1 179:0 0 3.6G 0 disk
└─mmcblk1p1 179:1 0 3.6G 0 part /
ubuntu@arm:~$
第一部分放:
u-boot.img MLO uImage zImage
第二部分放文件系统
第三部分未用
这个制作好的SD卡可以在Am335x-evm-sk上使用正常启动,但是在BeagleBone black却不能正常启动时什么原因?
启动调试信息:
U-Boot SPL 2016.03 (Oct 16 2017 - 19:22:35) preloader_console_init() >>spl:SDRAM_init() >>spl:board_init_r() MAIN_OSC: 24Mhz DPLL_Mpu_Freq: 300MHz DPLL_Core_Freq: 100MHz DPLL_Per_Freq_usb_phy_clk: 960MHz DPLL_Per_Freq_PRU_ICSS_Uart_moduclk: 192MHz DPLL_Per_Freq_MMC_moduclk: 96MHz DPLL_Per_Freq_SPI_moduclk: 48MHz DPLL_Per_Freq_UART_moduclk: 48MHz DPLL_Per_Freq_I2C_moduclk: 48MHz This is sure,only I think /arch/arm/cpu/armv7/omap-common/save_omap_boot_params /arch/arm/cpu/armv7/omap-common/gpmc_init /arch/arm/cpu/armv7/omap-common/i2c_init /arch/arm/cpu/armv7/omap-common/arch_misc_init() /arch/arm/cpu/armv7/omap-common/hw_watchdog_init() /arch/arm/cpu/armv7/omap-common/am33xx_spl_board_init() Trying to boot from MMC MMC->xxxx/drivers/mmc/mmc.c2 reading args spl_load_image_fat_os: error reading image args, err - -1 reading u-boot.img reading u-boot.img U-Boot 2016.03 (Oct 16 2017 - 19:22:35 +0800) U-Boot code: 80800000 -> 808DA324 BSS_END: -> 80926BBC Watchdog enabled I2C: ready DRAM: 512 MiB NAND: 0 MiB nand_init->xxxx/drivers/mtd/nand/nand.c MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 MMC->xxxx/drivers/mmc/mmc.c1 MMC->xxxx/drivers/mmc/mmc.c2 xxxx/common/env_common.c *** Error - No Valid Environment Area found *** Warning - bad CRC, using default environment xxxx/common/env_common.c Net: xxx/board/ti/am335x/board_eth_init--->,6be7 xxx/board/ti/am335x/board_eth_init--->,5fab5ef4 <ethaddr> not set. Validating first E-fuse MAC Here at xxx/drivers/net/cpsw.c phy_reg---> 3000 phy_reg---> 7809 phy_reg---> 7 phy_reg---> c0f1 phy_reg---> 1e1 phy_reg---> 1 phy_reg---> 0 phy_reg---> ffff phy_reg---> ffff phy_reg---> ffff phy_reg---> ffff phy_reg---> ffff phy_reg---> ffff phy_reg---> ffff phy_reg---> ffff phy_reg---> 0 phy_reg---> 40 phy_reg---> 2 phy_reg---> e0 phy_reg---> ffff phy_reg---> 0 phy_reg---> 0 phy_reg---> 0 phy_reg---> 0 phy_reg---> ffff phy_reg---> ffff phy_reg---> 0 phy_reg---> 0 phy_reg---> 0 phy_reg---> 90 phy_reg---> 0 phy_reg---> 40 End xxx/Board/Ti/Am335x/Board.c:---->Ethernet_init maria: ----> 40070106 maria: ----> 410000ff maria: ----> 1 maria: ----> 0 maria: ----> 0 maria: ----> 0 maria: ----> 1 maria: ----> 0 maria: ----> 0 maria: ----> 0 maria: ----> 23e00040 maria: ----> 0 maria: ----> 0 maria: ----> 0 xxx/Board/Ti/Am335x/Board.c:---->Ethernet_init cpsw, usb_ether NET: -> xxxx/net/eth_legacy.c Press SPACE to abort autoboot in 5 seconds ## Error: "envboot" not defined lcd reset switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt 133 bytes read in 4 ms (32.2 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... Running uenvcmd ... reading uImage 4287776 bytes read in 391 ms (10.5 MiB/s) reading zyr-am335x-evmsk.dtb 32012 bytes read in 15 ms (2 MiB/s) ## Booting kernel from Legacy Image at 82000000 ... Image Name: Linux-3.14.65 Created: 2017-06-12 5:13:43 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 4287712 Bytes = 4.1 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK ## Flattened Device Tree blob at 83000000 Booting using the fdt blob at 0x83000000 Loading Kernel Image ... OK Loading Device Tree to 8fff5000, end 8ffffd0b ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 3.14.65 (zyr@ubuntu) (gcc version 4.6.3 (Ubuntu/Linar o 4.6.3-1ubuntu5) ) #1 SMP Mon Jun 12 12:35:16 CST 2017 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x EVM-SK [ 0.000000] cma: CMA: reserved 16 MiB at 9e800000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon ) [ 0.000000] PERCPU: Embedded 9 pages/cpu @dfad4000 s13184 r8192 d15488 u36864 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages : 129792 [ 0.000000] Kernel command line: root=/dev/mmcblk0p2 rootwait console=ttyO0,115 200 [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 487848K/523264K available (5629K kernel code, 655K rwdata, 2132K rodata, 384K init, 5518K bss, 35416K reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc079c71c (7762 kB) [ 0.000000] .init : 0xc079d000 - 0xc07fd380 ( 385 kB) [ 0.000000] .data : 0xc07fe000 - 0xc08a1e18 ( 656 kB) [ 0.000000] .bss : 0xc08a1e18 - 0xc0e05968 (5519 kB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1 [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000010] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 1789569 69942ns [ 0.000055] OMAP clocksource: timer1 at 24000000 Hz [ 0.000818] Console: colour dummy device 80x30 [ 0.000871] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo M olnar [ 0.000879] ... MAX_LOCKDEP_SUBCLASSES: 8 [ 0.000887] ... MAX_LOCK_DEPTH: 48 [ 0.000894] ... MAX_LOCKDEP_KEYS: 8191 [ 0.000901] ... CLASSHASH_SIZE: 4096 [ 0.000908] ... MAX_LOCKDEP_ENTRIES: 16384 [ 0.000915] ... MAX_LOCKDEP_CHAINS: 32768 [ 0.000922] ... CHAINHASH_SIZE: 16384 [ 0.000930] memory used by lock dependency info: 3695 kB [ 0.000937] per task-struct memory footprint: 1152 bytes [ 0.000980] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.079153] pid_max: default: 32768 minimum: 301 [ 0.079511] Security Framework initialized [ 0.079624] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.079637] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.098616] CPU: Testing write buffer coherency: ok [ 0.099959] CPU0: thread -1, cpu 0, socket -1, mpidr 0 [ 0.100031] Setting up static identity map for 0x80556c28 - 0x80556c98 [ 0.102994] Brought up 1 CPUs [ 0.103014] SMP: Total of 1 processors activated (996.14 BogoMIPS). [ 0.103024] CPU: All CPU(s) started in SVC mode. [ 0.105719] devtmpfs: initialized [ 0.115227] VFP support v0.3: implementor 41 architecture 3 part 30 variant c r ev 3 [ 0.149938] omap_hwmod: tptc0 using broken dt data from edma [ 0.150292] omap_hwmod: tptc1 using broken dt data from edma [ 0.150632] omap_hwmod: tptc2 using broken dt data from edma [ 0.158277] omap_hwmod: debugss: _wait_target_disable failed [ 0.217074] pinctrl core: initialized pinctrl subsystem [ 0.221344] regulator-dummy: no parameters [ 0.224651] NET: Registered protocol family 16 [ 0.229775] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.247475] platform 49000000.edma: alias fck already exists [ 0.247514] platform 49000000.edma: alias fck already exists [ 0.247532] platform 49000000.edma: alias fck already exists [ 0.251781] OMAP GPIO hardware version 0.1 [ 0.281185] No ATAGs? [ 0.281211] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.339642] bio: create slab <bio-0> at 0 [ 0.378631] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver [ 0.380895] vbat: 5000 mV [ 0.382043] lis3_reg: no parameters [ 0.388837] SCSI subsystem initialized [ 0.392242] usbcore: registered new interface driver usbfs [ 0.392683] usbcore: registered new interface driver hub [ 0.393425] usbcore: registered new device driver usb [ 0.396284] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e1 0800/pinmux_i2c0_pins, deferring probe [ 0.396328] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral [ 0.403461] Switched to clocksource timer1 [ 0.556282] NET: Registered protocol family 2 [ 0.558293] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.558476] TCP bind hash table entries: 4096 (order: 5, 147456 bytes) [ 0.559840] TCP: Hash tables configured (established 4096 bind 4096) [ 0.559991] TCP: reno registered [ 0.560016] UDP hash table entries: 256 (order: 2, 20480 bytes) [ 0.560206] UDP-Lite hash table entries: 256 (order: 2, 20480 bytes) [ 0.561159] NET: Registered protocol family 1 [ 0.562505] RPC: Registered named UNIX socket transport module. [ 0.562526] RPC: Registered udp transport module. [ 0.562535] RPC: Registered tcp transport module. [ 0.562544] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.563832] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available [ 0.572179] futex hash table entries: 256 (order: 2, 16384 bytes) [ 0.713326] VFS: Disk quotas dquot_6.5.2 [ 0.713776] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.715791] NFS: Registering the id_resolver key type [ 0.716173] Key type id_resolver registered [ 0.716194] Key type id_legacy registered [ 0.716313] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.716726] msgmni has been set to 984 [ 0.719690] io scheduler noop registered [ 0.719713] io scheduler deadline registered [ 0.719787] io scheduler cfq registered (default) [ 0.722742] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.727139] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.734768] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.736026] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 30 00000) is a OMAP UART0 [ 1.395813] console [ttyO0] enabled [ 1.405702] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 1.442961] brd: module loaded [ 1.464960] loop: module loaded [ 1.474411] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.489262] usbcore: registered new interface driver asix [ 1.495915] usbcore: registered new interface driver ax88179_178a [ 1.502698] usbcore: registered new interface driver cdc_ether [ 1.509374] usbcore: registered new interface driver smsc95xx [ 1.516261] usbcore: registered new interface driver net1080 [ 1.522580] usbcore: registered new interface driver cdc_subset [ 1.529264] usbcore: registered new interface driver zaurus [ 1.535718] usbcore: registered new interface driver cdc_ncm [ 1.543884] usbcore: registered new interface driver cdc_wdm [ 1.550304] usbcore: registered new interface driver usb-storage [ 1.557154] usbcore: registered new interface driver usbtest [ 1.566986] mousedev: PS/2 mouse device common for all mice [ 1.578298] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.585937] 44e3e000.rtc: already running [ 1.591466] i2c /dev entries driver [ 1.595905] Driver for 1-wire Dallas network protocol. [ 1.606221] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.617699] omap_hsmmc 48060000.mmc: vmmc regulator missing [ 1.624183] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral [ 1.633908] usbcore: registered new interface driver usbhid [ 1.639737] usbhid: USB HID core driver [ 1.646188] oprofile: using arm/armv7 [ 1.650668] TCP: cubic registered [ 1.654264] Initializing XFRM netlink socket [ 1.658851] NET: Registered protocol family 17 [ 1.663617] NET: Registered protocol family 15 [ 1.668591] Key type dns_resolver registered [ 1.675190] ThumbEE CPU extension supported. [ 1.679703] Registering SWP/SWPB emulation handler [ 1.688582] lis3_reg: disabling [ 1.691885] vbat: disabling [ 1.694911] regulator-dummy: disabling [ 1.706831] tps65910 0-002d: No interrupt support, no core IRQ [ 1.716819] tps65910 0-002d: Error in configuring external control EN1 [ 1.723756] tps65910 0-002d: Failed to initialise ext control config [ 1.731886] vrtc: failed to enable [ 1.738066] tps65910 0-002d: failed to register tps65910-pmic regulator [ 1.745181] tps65910-pmic: probe of tps65910-pmic failed with error -121 [ 1.756782] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.764271] omap_hsmmc 48060000.mmc: vmmc regulator missing [ 1.770355] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral [ 1.843468] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6 [ 1.849853] davinci_mdio 4a101000.mdio: detected phy mask fffffffe [ 1.858931] libphy: 4a101000.mdio: probed [ 1.863141] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720 [ 1.874445] omap_hsmmc 48060000.mmc: vmmc regulator missing [ 1.880513] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral [ 1.889233] Detected MACID = f4:5e:ab:5f:e7:6b [ 1.896830] omap_hsmmc 48060000.mmc: vmmc regulator missing [ 1.902886] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral [ 1.914025] omap_hsmmc 48060000.mmc: vmmc regulator missing [ 1.920090] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral [ 1.930453] input: gpio_buttons.7 as /devices/gpio_buttons.7/input/input0 [ 1.941590] omap_hsmmc 48060000.mmc: vmmc regulator missing [ 1.947852] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral [ 1.956030] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:37:19 UTC (946687039) [ 1.984506] Waiting for root device /dev/mmcblk0p2...
内核中配置支持ext3,ext4.
浏览论坛有的说是硬件问题,我试着吧CD脚给注释还是不行这是这么原因呢?
这种情况,往往是因为kernel中对于CD脚的检测逻辑导致了停在那里。你把CD脚注释掉了,是只是注释掉了pinmux中关于MMC_CD的配置,还是把kernel中的那个CD检测逻辑也注释掉了?
应该是在加载文件系统时内核没有找到文件的位置。试着修改uEnv.txt里的环境变量,为题解决