This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何使用TMDSEVM6678LE上面的xds560v2调试自己定制的TMS320C6678板卡?



定制板卡上面可能会有2~4个DSP,如何使用TMDSEVM6678LE上面的xds560v2调试?EMU信号该如何处理?

  • 可以参考下面到链接。

    http://processors.wiki.ti.com/index.php/Connect_2%2B_Chips_With_Emulator

    http://processors.wiki.ti.com/index.php/XDS_Target_Connection_Guide#Multiple_Devices

  • Shine Zhang 你好:

           我现在想用6678评估板上面的Blackhawk XDS560v2-USB Mezzanine Emulator这个仿真器。在我的定制板卡上面放一个60针的调试头,然后将这个仿真器放在我的定制板卡上面,这样能否行的通?仿真器是否需要一些额外的配置?

  • 每个板子都有一个配置文件.xxcml, 里面需要配置JTAG调试链的配置信息,还需要加载板卡硬件初始化相关的脚本文件.gel,包括板子上锁相环PLL以及DDR的相关配置初始化操作。6678标准板卡这些文件在TI CCS IDE里面都有提供,但是如果是定制板卡的话,这些文件都要单独自己配置(.xxcml)或者是编写(.gel),否则无法通过仿真器加载成功。所以对于定制板来说,还是有一部分工作要做的。

    Best Regards,

    Martin