各位专家,如题,中文和英文网站都无法下载,请问怎么办?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位专家,如题,中文和英文网站都无法下载,请问怎么办?
可以打开的,你要下哪个版本?
DSP/BIOS Product Releases | |
DSP/BIOS 5.42.02.10 | Added TMS320C5545 support with boost5545 platform. There are no target content changes in this release. See release notes |
DSP/BIOS 5.42.01.09 | Exactly the same as 5.42.00.07 except for some installer updates for CCSv5.4.0. See release notes for details. |
DSP/BIOS 5.42.00.07 | Removes support for CCSv3.x. Adds 5517 support. Includes tconf utility (no longer dependent on XDCtools for tconf). See release notes for details. |
DSP/BIOS 5.41.13.42 | Maintenance Release with minor bug fixes. See release notes for details. |
DSP/BIOS 5.41.12.40 | Maintenance Release with minor bug fixes. See release notes for details. |
DSP/BIOS 5.41.11.38 | TSPA-licensed DSP/BIOS patch release compatible with CCS 5.1, 4.2.4 and CCS 3.3. Adds support for 5525 and 553x devices. Updated eclipse plugins to work with CCSv5.1 beta2 and later. No other bug fixes. There’s no reason to update to this release unless you are using one of these new devices. See release notes for details. |
DSP/BIOS 5.41.10.36 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.09.34 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.08.30 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.07.24 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.06.21 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.05.20 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.04.18 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.03.17 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.02.14 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS5.41.01.09 | TSPA-licensed DSP/BIOS patch release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.41.00.06 | TSPA-licensed DSP/BIOS release compatible with CCS 4.0 and CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.40.03.23 | TSPA-licensed DSP/BIOS release compatible with CCS 4.0. Not compatible with C672x ROM image. No 54x support in this release. |
DSP/BIOS 5.33.06 | TSPA-licensed DSP/BIOS release compatible with CCS 3.3. Not compatible with C672x ROM image. No 54x support in this release. |
Previous Releases | Earlier Releases (link requires TI&ME login). |