各位好:
在调试AM3358时遇到一个问题,经过测试发现主电掉电后,备电供电,然后TPS65910-VBAT上可以测量到0.4V的电压,不清楚这个电压是怎么来的,请帮忙分析下。我们使用外部程控电源1.8V直接给RTC供电,然后发现依旧有VBAT依旧有0.4V的电压,功耗有100Ua以上.而摘掉PMU,直接用1.8V给RTC供电,则VBAT没有0.4V的电压,RTC的功耗也几乎不可计。
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我的电脑为什么总是不能发新帖,只能到贴里面恢复才能发言!!!
我想问的是,我新做了个AM3352的板子,跟以前的旧板相差不大!但是以访问内部RTC相关的寄存器等等就程序跑飞,指令直接跳到了0x80000010的地方了!如果没有访问RTC相关的东西没有问题正常工作!直接使用TI提供的RTC例程跑也是同样的问题,初始化RTC就跑飞了!这个VDDS_RTC电源1.795伏,量得CAP_VDD_RTC是1.1伏,认为正常。以前旧的板子没有问题可以正常访问RTC。想询问一下关于RTC跑飞的原因....