This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 vou1(HDMI)输出bt656 隔行PAL问题



首先,通过修改MCfw中HDMI(VOUT1)相关分辨率到SYS_STD_PAL,
然后,修改了VPPS系统中gSystem_dctrl的显示配置,
最后修改了在
vpshal_hdvenc.c中增加{{FVID2_STD_PAL, 720, 576, FVID2_SF_INTERLACED, 27000, 30, 12, 68, 64, 2, 19, 3}, 4, 4, 4},时序,
但是,实测,BT656 通过ADV7390后接屏,只有几秒钟有图像,而且图像不对,几秒后没有图像成蓝屏,
请问,我在vpshal_hdvenc.c中增加{{FVID2_STD_PAL, 720, 576, FVID2_SF_INTERLACED, 27000, 30, 12, 68, 64, 2, 19, 3}, 4, 4, 4},时序对吗?
DM8168对于Vout1 输出bt656隔行视频标准时序是什么,有没有Vout1输出BT656的例子,
该问题如何定位,请大家帮忙

  • 该问题有了进展了,如下图

  • 请各位前辈高人指点,上图中只有一部分图像胡原因,主要的显示代码如下,谢谢大家。

    (1)app部分主要代码
    for(i=0; i<1; i++)
    {
    swMsPrm[i].inQueParams.prevLinkId = SYSTEM_VPSS_LINK_ID_DUP_0;
    swMsPrm[i].inQueParams.prevLinkQueId = 1;
    swMsPrm[i].outQueParams.nextLink = gVdisModuleContext.displayId[0];
    swMsPrm[i].maxInputQueLen = SYSTEM_SW_MS_DEFAULT_INPUT_QUE_LEN;
    swMsPrm[i].maxOutRes = VSYS_STD_PAL;
    swMsPrm[i].initOutRes = VSYS_STD_PAL;
    swMsPrm[i].lineSkipMode = FALSE;
    swMsPrm[i].enableLayoutGridDraw = FALSE;
    swMsPrm[i].numOutBuf = 4;
    swMsPrm[i].enableProcessTieWithDisplay = TRUE;
    swMsPrm[i].outDataFormat = SYSTEM_DF_YUV422I_YUYV;
    swMsPrm[i].outputBufModified = TRUE;
    MultiCh_swMsGetDefaultLayoutPrm_k1774_PAL(0, &swMsPrm[i], FALSE); /* Since only live preview is there, show it on both displays */
    }


    DisplayLink_CreateParams prm_dis;
    MULTICH_INIT_STRUCT(DisplayLink_CreateParams, prm_dis);
    prm_dis.inQueParams[0].prevLinkId = gVdisModuleContext.swMsId[0];
    prm_dis.inQueParams[0].prevLinkQueId = 0;
    prm_dis.displayRes = VSYS_STD_PAL;



    (2)mcfw

    ti_vdis.c

    pContext->deviceParams[VDIS_DEV_HDMI].enable = TRUE;
    pContext->deviceParams[VDIS_DEV_HDMI].outputInfo.vencNodeNum = VDIS_VENC_HDMI;
    pContext->deviceParams[VDIS_DEV_HDMI].outputInfo.aFmt = VDIS_A_OUTPUT_COMPOSITE;
    pContext->deviceParams[VDIS_DEV_HDMI].outputInfo.dvoFmt = VDIS_DVOFMT_SINGLECHAN;
    pContext->deviceParams[VDIS_DEV_HDMI].outputInfo.dataFormat = SYSTEM_DF_YUV422SP_UV;

    system_dctrl.c

    Vps_DcConfig gSystem_dctrlTriDisplayConfigDvo2 = {
    VPS_DC_USERSETTINGS, /* Use Case */
    /* Edge information */
    {
    {VPS_DC_BP0_INPUT_PATH, VPS_DC_VCOMP_MUX} ,
    {VPS_DC_VCOMP_MUX, VPS_DC_VCOMP} ,
    {VPS_DC_CIG_NON_CONSTRAINED_OUTPUT, VPS_DC_HDMI_BLEND} ,
    {VPS_DC_BP1_INPUT_PATH, VPS_DC_HDCOMP_MUX} ,
    {VPS_DC_HDCOMP_MUX, VPS_DC_CIG_PIP_INPUT} ,
    {VPS_DC_CIG_PIP_OUTPUT, VPS_DC_DVO2_BLEND} ,
    {VPS_DC_CIG_PIP_OUTPUT, VPS_DC_HDCOMP_BLEND} ,
    {VPS_DC_SEC1_INPUT_PATH, VPS_DC_SDVENC_MUX} ,
    {VPS_DC_SDVENC_MUX, VPS_DC_SDVENC_BLEND} ,
    {VPS_DC_GRPX0_INPUT_PATH, VPS_DC_HDMI_BLEND} ,
    {VPS_DC_GRPX1_INPUT_PATH, VPS_DC_HDCOMP_BLEND} ,
    {VPS_DC_GRPX1_INPUT_PATH, VPS_DC_DVO2_BLEND},
    {VPS_DC_GRPX2_INPUT_PATH, VPS_DC_HDMI_BLEND}
    }
    ,
    13,
    /* VENC information */
    {
    /* Mode information */
    {
    {VPS_DC_VENC_HDMI, {FVID2_STD_PAL}
    }
    ,
    {VPS_DC_VENC_HDCOMP, {FVID2_STD_1080P_60}
    }
    ,
    {VPS_DC_VENC_DVO2, {FVID2_STD_1080P_60}
    }
    ,
    {VPS_DC_VENC_SD, {FVID2_STD_NTSC}
    }
    }
    ,
    (VPS_DC_VENC_DVO2 | VPS_DC_VENC_HDCOMP), /* Tied VENC bit
    * mask */
    4u /* Number of VENCs
    */
    }
    };

    (3)hdvpss
    vpshal_hdvenc.c
    {{FVID2_STD_PAL, 1442, 576, FVID2_SF_INTERLACED, 27000, 25,
    12, 140, 64, 2, 19, 3}, 4, 4, 4},