This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一下:6655的PCIe,必须要使用RTOS系统吗?



想用6655的PCIe x2,是必须要使用RTOS系统才行吗?可以脱离系统,只用裸片实现PCIe的接口吗?

新手提问,请大牛指点。

  • 不是必须的。可以参考置顶贴里c6657的例程。
    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/47664.aspx?pi239031348=2

  • 你好,谢谢你,我下载到了你说的那个文件。还有两个问题请教,谢谢了。

    1、6657芯片中是不是没有程序存储器,是不是必须要外接flash才能存入程序?

    2、如果使用外接的flash程序存储器,如何从外部设备启动呢?有没有这样的例程或者手册可以供我参考?我想外接一个flash存储器(通过SPI或者EMIF外接)作为程序存储器,谢谢!

  • 你可以参考一下这个帖子:

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/142834.aspx