This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320TCI6614 PIN脚定义的说明文档能提供一份吗?

手上有一块TMS320TCI6614EVM的开发板,但缺少了相关的资料光盘,TI官网上能下载的资料非常有限,直接介绍TMS320TCI6614这颗DSP的文档就只有:sprs671c.pdf这个文档,翻遍所有资料也没找到DSP的各个管脚定义的信息。能否提供一份详细的TMS320TCI6614的说明文档?

另外:

TMS320TCI6614

0x0080_0000 到0x008F_FFFF定义了L2   SRAM

0x00E0_0000 到0x00E0_7FFF定义了L1P SRAM

0x00F0_0000 到0x00F0_7FFF定义了L1D SRAM

请问这个一二级缓存是属于DSP的哪个执行单元的?

因为后面已经定义了DSP CorePac0/1/2/3以及ARM的缓存地址,所以我对此非常疑惑。

万分感谢

  • TCI6614资料:www.ti.com/.../tms320tci6614

    EVM6614资料:www.advantech.com/.../TI-EVM

    你所提到的管脚说明在你所看到的文档的2.11节。

    一二级缓存是corepac内部L1及L2  memory,你所列出的地址范围仅是对于该核可见的局部地址,后续如0x10800000的地址是全局地址,在使用过程中如果其他核、EDMA或者外设在访问L1及L2需要使用全局地址。

  • 不好意思,前一个问题,管脚说明我已经找到了,自己没留意看。

  • 关于第二个问题,我还是没有弄明白,根据文档:

    0x0080_0000 到0x008F_FFFF   L2   SRAM

    0x00E0_0000 到0x00E0_7FFF  L1P SRAM

    0x00F0_0000 到0x00F0_7FFF   L1D SRAM

    和后面CorePac0/1/2/3的一二级缓存并不重叠

    全局和局部的说法我还是无法理解,能更详细说明下吗?

    CorePac0/1/2/3的一二级缓存都已经如下定义

    1080 0000 108F FFFF 0 1080 0000 0 108F FFFF 1M CorePac0 L2 SRAM

    1090 0000 10DF FFFF 0 1090 0000 0 10DF FFFF 5M Reserved

    10E0 0000 10E0 7FFF 0 10E0 0000 0 10E0 7FFF 32k CorePac0 L1P SRAM

    10E0 8000 10EF FFFF 0 10E0 8000 0 10EF FFFF 1M-32K Reserved

    10F0 0000 10F0 7FFF 0 10F0 0000 0 10F0 7FFF 32k CorePac0 L1D SRAM

    10F0 8000 117F FFFF 0 10F0 8000 0 117F FFFF 9M-32k Reserved

    1180 0000 118F FFFF 0 1180 0000 0 118F FFFF 1M CorePac1 L2 SRAM

    1190 0000 11DF FFFF 0 1190 0000 0 11DF FFFF 5M Reserved

    11E0 0000 11E0 7FFF 0 11E0 0000 0 11E0 7FFF 32k CorePac1 L1P SRAM

    11E0 8000 11EF FFFF 0 11E0 8000 0 11EF FFFF 1M-32K Reserved

    11F0 0000 11F0 7FFF 0 11F0 0000 0 11F0 7FFF 32k CorePac1 L1D SRAM

    11F0 8000 127F FFFF 0 11F0 8000 0 127F FFFF 9M-32k Reserved

    1280 0000 128F FFFF 0 1280 0000 0 128F FFFF 1M CorePac2 L2 SRAM

    1290 0000 12DF FFFF 0 1290 0000 0 12DF FFFF 5M Reserved

    12E0 0000 12E0 7FFF 0 12E0 0000 0 12E0 7FFF 32k CorePac2 L1P SRAM

    12E0 8000 12EF FFFF 0 12E0 8000 0 12EF FFFF 1M-32K Reserved

    12F0 0000 12F0 7FFF 0 12F0 0000 0 12F0 7FFF 32k CorePac2 L1D SRAM

    12F0 8000 137F FFFF 0 12F0 8000 0 137F FFFF 9M-32k Reserved

    1380 0000 1388 FFFF 0 1380 0000 0 1388 FFFF 1M CorePac3 L2 SRAM

    1390 0000 13DF FFFF 0 1390 0000 0 13DF FFFF 5M Reserved

    13E0 0000 13E0 7FFF 0 13E0 0000 0 13E0 7FFF 32k CorePac3 L1P SRAM

    13E0 8000 13EF FFFF 0 13E0 8000 0 13EF FFFF 1M-32K Reserved

    13F0 0000 13F0 7FFF 0 13F0 0000 0 13F0 7FFF 32k CorePac3 L1D SRAM

  • 简单理解就是0x00800000与0x10800000对应相同的物理地址,只是0x00800000是只局限于core在访问本核L1、L2时可用,而其他master在访问L1/L2时必须使用0x10800000的全局地址。不要想得太复杂。

  • 谢谢!

    我还想再深入了解下:TMS320TCI6614有4个DSP核和1个A8 ARM核,前面的一二级缓存对应4个DSP核中的哪一个是怎么决定的呢?