在实际使用中,需要DSP与FPGA之间通过SRIO通信。DSP与FPGA之间同时有两组数据进行传输。DSP可以设置为2个2x,2个port分别为0和2,而FPGA例化2个2x时,端口号应该都默认是0吧,并且FPGA中的2个srio的地址应该不同吧?如果可以这样设置,DSP端怎么区分FPGA中的两个SRIO发送来的门铃信号?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在实际使用中,需要DSP与FPGA之间通过SRIO通信。DSP与FPGA之间同时有两组数据进行传输。DSP可以设置为2个2x,2个port分别为0和2,而FPGA例化2个2x时,端口号应该都默认是0吧,并且FPGA中的2个srio的地址应该不同吧?如果可以这样设置,DSP端怎么区分FPGA中的两个SRIO发送来的门铃信号?
您好,我也遇到同样的问题,我实际出现的现象是:FPGA1向DSP发送数据时,门铃包和数据都没有问题;但是FPGA2向FPGA发送数据时,DSP只能收到数据而收不到门铃包。向问下您这个问题有没有解决呢?