omapl138的上电时序是1.3-》1.8-》1.2吗?现在1.8V被强制拉到了2.7V,断开1.8V与外界的连接,发现1.8V输出正常。
看了之前大家遇到过类似的问题,尝试并联电阻,没有解决问题。
请问,上电时序是什么?1.8V被拉到2.7V该怎么解决?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
omap-l138的上电顺序是1.3v->1.8v->3.3v,具体可以看数据手册第83页上的说明。
6.3.1 Power-On Sequence
http://www.ti.com/lit/ds/symlink/omap-l138.pdf
1.8v被强制拉到2.7v是因为1.8V上的电容不够,和3.3V上电爬坡太慢造成的,解决方法可以参考下面的勘误表。
Advisory 2.3.18 DVDD18 Can Pull Up to 2.7V When Using Dual-Voltage IOs at 3.3V
http://www.ti.com/lit/er/sprz301m/sprz301m.pdf