This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148/DM8168 IVAHD 通道关联关系



大家好!

在阅读 DVRRDK 代码的时候发现有设置 IVAHD 通道的代码 如下:

static SystemVideo_Ivahd2ChMap_Tbl systemVid_encDecIvaChMapTbl =
{
.isPopulated = 1,
.ivaMap[0] =
{
.EncNumCh = 10,
.EncChList = {0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 0, 0, 0, 0 , 0, 0},
.DecNumCh = 0,
.DecChList = {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0},
},
.ivaMap[1] =
{
.EncNumCh = 0,
.EncChList = {16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31},
.DecNumCh = 12,
.DecChList = {0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 0, 0 , 0, 0},
},
.ivaMap[2] =
{
.EncNumCh = 6,
.EncChList = {10, 11, 12, 13, 14, 15, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0},
.DecNumCh = 4,
.DecChList = {12, 13, 14, 15, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0},
},
};

初步了解到是设置3个视频加速器通道对应关系的,但是具体要深入理解这些参数含义或者机制的话,如 EncChList = {0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 0, 0, 0, 0 , 0, 0},

有哪些文档有涉及可以参考的,望TI的大神们给个建议。

  • /**
       \brief Data structure to assign the video channles to any single IVA-HD
    */
    typedef struct SystemVideo_Ivahd2ChMap {
        UInt32 EncNumCh;  
        /**< Number of Encoder channels */
        UInt32 EncChList[SYSTEMVIDEO_MAX_IVACH];
        /**< Encoder channel list */
        UInt32 DecNumCh;
        /**< Number of Decoder channels */
        UInt32 DecChList[SYSTEMVIDEO_MAX_IVACH];
        /**< Decoder channel list */
    } SystemVideo_Ivahd2ChMap;
  • typedef struct SystemVideo_Ivahd2ChMap_Tbl {
    UInt32 isPopulated;
    /**< Flag to verify if the table is populated */
    SystemVideo_Ivahd2ChMap ivaMap[SYSTEMVIDEO_MAX_NUMHDVICP];
    /**< Structure to assign the video channels to all 3 IVA-HDs */
    } SystemVideo_Ivahd2ChMap_Tbl;

    你好;

           这里 3个 ivaMap ,分别代表 dm8168 中的 3个 hdvicp 视频编码引擎,

        EncChList  这里是encode link 中对应的编码通道的 id;
        注意资源的合理使用就行,保证性能满意要求就可以;
  • HI, :

      请教下,ti有没有相关的文档对这块有介绍的?

  • 没有文档专门针对这部分的介绍;

    理解起来其实是比较容易;有部分资料可以参考,都有简单提到:

    HDVICP20_API_UserGuide.pdf

    DVR_RDK_ApiGuide.CHM

    DVR_RDK_McFW_Link_API_Training.pdf