This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教C6657的SRIO boot方式



我的板子上有2个DSP,都是6657。其中一个要用SRIO方式启动,另一个SPI启动。SPI启动的DSP正常工作,另一个DSPoot 模式已经正确设置为SRIO 模式(该DSP的boot mode的参考时钟、端口速率、lane模式的管脚都确认正确的),但是2个DSP之间SRIO链路不通;如果把SRIO启动方式这个DSP 的boot模式修改为NO BOOT模式,通过DSP仿真器加载代码运行,则2个DSP之间的SRIO链路是通的,说明硬件链路是没有问题的。请教搞过SRIO boot方式的大牛,可能会是神马原因?是否跟对端的SRIO初始化配置有关系?