您好,请教一下
在DM8168的上使用TVP5158采集640 x 480视频,对视频标准standard赋值SYSTEM_STD_MUX_4CHD1,采集模式是多路复用可以正常采集视频。
当视频标准standard赋值SYSTEM_STD_D1,采集模式是单路时,采集不到数据,不知是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请教一下
在DM8168的上使用TVP5158采集640 x 480视频,对视频标准standard赋值SYSTEM_STD_MUX_4CHD1,采集模式是多路复用可以正常采集视频。
当视频标准standard赋值SYSTEM_STD_D1,采集模式是单路时,采集不到数据,不知是什么原因?
你好,
Tvp5158的输入是ntsc或pal,不会是640x480的分辨率。
您好,谢谢您的回复
现在采集的视频是NTSC(720x480),但是编码和显示的都只有一半视频(720x240),一半灰屏(720x240),请教一下,这是什么原因导致?
建议了解了 480i 和 480p 的区别。
NTSC 是 480i 视频。
谢谢您的回复,如果输入是640x480,经过TVP5158是否放大为720x576?
您好,谢谢您的回复
这是拍的图片,现在可以正常显示,但是影响另一路1080P的rtsp视频流传输,丢帧特别厉害。
请教一下,输入视频是逐行的,采集配置是隔行的有什么影响?