This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP-SDK 在 am57xx SDK上编译,出现flycapture问题

【错误】

Nothing PROVIDES 'flycapture' (but /home/mike/work/testeye/tisdk/sources/meta-processor-sdk/recipes-ee/dlp-sdk/dlp-sdk_2.0.bb DEPENDS on or otherwise requires it)

【步骤】

1、已经编译了MACHINE=am57xx-evm bitbake arago-core-tisdk-image

2、已经将dlp-sdk 和flycapture的包按照下面命令放在相关位置

3、执行MACHINE=am57xx-evm bitbake dlp-sdk   则出现最上面的错误打印信息,  感觉flycapture的SDK需要配置一下??

1. Refer to Processor SDK - Building the SDK at processors.wiki.ti.com/.../Processor_SDK_Building_The_SDK, to set up the build environment and get familiar with how to use Bitbake. Ensure to build arago-core-tisdk-image (MACHINE=am57xx-evm bitbake arago-core-tisdk-image);

2. Download the DLP-SDK source tarball (dlp-sdk-2.0.tar.gz) of this design guide from: www.ti.com/.../TIDEP0076.

3. Place this tarball under the oe-layersetup/downloads directory, and touch oe-layersetup/downloads/dlpsdk-2.0.tar.gz.done.

4. The recipe (dlp-sdk_2.0.bb) for building the DLP-SDK from the release tarball is also located under the design file folder at: (www.ti.com/.../TIDEP0076). Create the folder oe-layersetup/sources/metaprocessor-sdk/recipes-ee/dlp-sdk, and place the recipe above there.

5. The DLP-SDK has dependency on FlyCapture (Point Grey ARMv7 Linux shared libraries). They are released under commercial license and can be obtained from Point Grey only. Download FlyCapture.2.9.3.43_armhf.tar.gz from www.ptgrey.com/.../downloads.

6. Place the tarball under the oe-layersetup/downloads directory, and touch oelayersetup/downloads/flycapture.2.9.3.43_armhf.tar.gz.done

7. Bitbake the dlp-sdk recipe: MACHINE=am57xx-evm bitbake dlp-sdk