尊敬的TI工程师和社区会员,你们好,我最近买了TMS320C6657Lite评估版,帮助老师做一些信号处理算法方面的验证,以便于后续的开发。其中使用到EDMA3将数据从DDR3传输到L2 Cache,产生了三个问题:
1.EDMA3 Low Level Driver是不是一定需要配合SYS/BIOS才能够使用,RTSC工程是否也一定需要SYS/BIOS组件;
2.在使用CSL中EDMA3的API实现数据搬移时,最后48个字节总是没有传输,无论怎样改变数据大小和数据类型,代码附在后面,我使用的是CCS5.4,pdk_C6657_1_1_2_6(代码是L2到L2的数据搬移,软件仿真和硬件上运行都是一样的问题);
3.pdk_C6657_1_1_2_6和pdk_c665x_2_0_4似乎改版很大?
问题2的代码:
/*
* main.c
*/
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <time.h>
#include <c6x.h>
#include <ti/csl/csl_edma3.h>
// for C6657, CSL_EDMA3 instance is No. 2
#define CSL_EDMA3 2
#define CSL_EDMA3_PARAM_0 0
#define CSL_EDMA3_TCC_0 CSL_EDMA3_PARAM_0
// data size
#define DATASIZE 128
Int main(void) {
// edma3 instance and pointer
CSL_Edma3Handle hModule;
CSL_Edma3Obj edmaObj;
// CSL function return
CSL_Status status;
// global or shadow region
CSL_Edma3CmdDrae regionAccess;
CSL_Edma3CmdIntr regionIntr;
// channel
CSL_Edma3ChannelObj chObj;
CSL_Edma3ChannelHandle hChannel;
CSL_Edma3ChannelAttr chAttr;
// param
CSL_Edma3ParamHandle hParamBasic;
CSL_Edma3ParamSetup myParamSetup;
// test data
Int srcBuff[DATASIZE];
Int dstBuff[DATASIZE];
Int i;
for(i = 0; i < DATASIZE; i++){
srcBuff[i] = i;
dstBuff[i] = 0;
}
// module initialization, always return CSL_SOK
CSL_edma3Init(NULL);
// module level open
hModule = CSL_edma3Open(&edmaObj, CSL_EDMA3, NULL, &status);
if(hModule == NULL || status != CSL_SOK){
printf("Edma module open failed\n");
return 0;
}
// DRAE Enable(Bits 0-15) for the Shadow Region 0.
regionAccess.region = CSL_EDMA3_REGION_0;
regionAccess.drae = 0xFFFF;
regionAccess.draeh = 0x0000;
status = CSL_edma3HwControl(hModule, CSL_EDMA3_CMD_DMAREGION_ENABLE, ®ionAccess);
if(status != CSL_SOK){
printf("Edma region enable command failed\n");
return 0;
}
// Channel 0 Open in context of Shadow region 0
chAttr.regionNum = CSL_EDMA3_REGION_0;
chAttr.chaNum = 0;
hChannel = CSL_edma3ChannelOpen(&chObj, CSL_EDMA3, &chAttr, &status);
if(hChannel == NULL || status != CSL_SOK){
printf("Edma channel open failed\n");
return 0;
}
// channel setup
status = CSL_edma3HwChannelSetupParam(hChannel, CSL_EDMA3_PARAM_0);
if(status != CSL_SOK){
printf("Edma channel setup param failed\n");
return 0;
}
// obtain a handle to param set 0
hParamBasic = CSL_edma3GetParamHandle(hChannel, 0, &status);
if(hParamBasic == NULL){
printf("Edma get param handle for param entry 0 failed\n");
return 0;
}
// channel default queue set to be 0
status = CSL_edma3HwChannelSetupQue(hChannel, CSL_EDMA3_QUE_0);
if(status != CSL_SOK){
printf("Edma channel setup que failed\n");
return 0;
}
// setup the parameter set
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS,
CSL_EDMA3_TCCH_DIS,
CSL_EDMA3_ITCINT_DIS,
CSL_EDMA3_TCINT_EN,
CSL_EDMA3_TCC_0,
CSL_EDMA3_TCC_NORMAL,
CSL_EDMA3_FIFOWIDTH_NONE,
CSL_EDMA3_STATIC_DIS,
CSL_EDMA3_SYNC_AB,
CSL_EDMA3_ADDRMODE_INCR,
CSL_EDMA3_ADDRMODE_INCR);
myParamSetup.srcAddr = (Uint32)srcBuff;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(DATASIZE,4);
myParamSetup.dstAddr = (Uint32)dstBuff;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(DATASIZE,DATASIZE);
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(CSL_EDMA3_LINK_NULL,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,0);
myParamSetup.cCnt = 1;
status = CSL_edma3ParamSetup(hParamBasic, &myParamSetup);
if(status != CSL_SOK){
printf("Edma parameter entry setup failed\n");
return 0;
}
// clear any pending event and then enable channel
status = CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_CLEAR,NULL);
if(status != CSL_SOK){
printf("Edma channel 0 clear failed\n");
return 0;
}
// Event enable
status = CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_ENABLE,NULL);
if(status != CSL_SOK){
printf("Edma channel 0 enable failed\n");
return 0;
}
// trigger channel 0
CSL_edma3HwChannelControl(hChannel, CSL_EDMA3_CMD_CHANNEL_SET, NULL);
// poll on interrupt bit 1
regionIntr.region = CSL_EDMA3_REGION_0;
while(1){
CSL_edma3GetHwStatus(hModule, CSL_EDMA3_QUERY_INTRPEND, ®ionIntr);
if(regionIntr.intr & (1<<CSL_EDMA3_PARAM_0)){
printf("capture interrupt\n");
break;
}
}
// clear interrupt bits
status = CSL_edma3HwControl(hModule, CSL_EDMA3_CMD_INTRPEND_CLEAR, ®ionIntr);
if(status != CSL_SOK){
printf("Edma, clear interrupt bits failed\n");
return 0;
}
for(i = 0; i < DATASIZE; i++){
if(srcBuff[i] != dstBuff[i]){
printf("*******************\ntransfer error\n********************\n");
break;
}
}
if(i == DATASIZE){
printf("transfer success\n");
}
// close channel
status = CSL_edma3ChannelClose(hChannel);
if(status != CSL_SOK){
printf("Edma channel close failed\n");
return 0;
}
// Close the Module.
status = CSL_edma3Close(hModule);
if(status != CSL_SOK){
printf("Edma module close failed\n");
return 0;
}
return 0;
}
包含的头文件和链接的库:
"${CG_TOOL_ROOT}/include"
"D:\ti\pdk_C6657_1_1_2_6\packages"
"libc.a"
"D:\ti\pdk_C6657_1_1_2_6\packages\ti\csl\lib\ti.csl.ae66"
cmd文件里指定以下选项避免printf出错,代码段和数据段都存储在L2 Cache中
-heap 0x8000
-stack 0xC000
产生的现象就是dstBuff里面只有1-115,后面是12个0。
另外,pdk_C6657_1_1_2_6包中的html说明文件有很多代码片段,但是却没有比较完整的例程,如果您能将一些常用的例程分享,将帮了我的大忙,非常感谢!我的邮箱是2455253013@qq.com