如下节点是uart1的节点,使用的是通道49,50,查看uart2,uart3,uart4,uart5... 它的序号并
不是连续的,另外,release的版本当中,uart8没有dmas属性,请教如何确定它的值呢,
目前 uart8已经正确配置pin mux,但是写数据时uart8_txd并没有信号输出,检查发现uart8
没有dmas属性。
59 uart1: serial@4806a000 {
60 compatible = "ti,omap4-uart";
61 reg = <0x4806a000 0x100>;
62 interrupts-extended = <&gic GIC_SPI 67 IRQ_TYPE_LEVEL_HIGH>;
63 ti,hwmods = "uart1";
64 clock-frequency = <48000000>;
65 status = "disabled";
66 /* Requesting crossbar input 49 and 50 */
67 dmas = <&sdma_xbar 49>, <&sdma_xbar 50>;
68 dma-names = "tx", "rx";
69 };
谢谢
BRs
Wufeng
15618297805