This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Nand启动DM8168,不成功,望赐教!



我的btmode[0,4]—10010,Nand启动DM8168,现有5块板,有1块板能从串口发出数据和FLASH有CS0片选动作,是不停输出0xF8 0x00 0xF8 0x00...,尝试 btmode[0,4]—01000,还是不停输出0xF8 0x00,NAND boot模式btmode[0,4]=01001,仍然不停输出0xF8 0x00...,NAND boot自启动模式时,用示波器观察,FLASH启动时,CS0有信号,D0,D6,D7始终为低电平,D1-D5有数据信号。

CCS中用仿真器读写FLASH测试,NAND是正常工作,而且此时用示波器观察,CS0有信号,D0-D7均有数据信号.

Bitwidth引脚即BTMODE12设置为0,8bit,FLASH型号MT29F4G08

  我们的CPU芯片系列号是
TMSDM8168ACYG,19AFVSW,786