Hi,大家好
请问 nRESETIN_OUT 复位信号 :输入输出是可以同时使用的吗? 如果不是,输入输出模式应该如何配置?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,大家好
请问 nRESETIN_OUT 复位信号 :输入输出是可以同时使用的吗? 如果不是,输入输出模式应该如何配置?
谢谢
不建议输入输出同时使用,请看TRM上的说明。
Caution must be used when implementing the nRESETIN_OUT as an bi-directional reset signal. Because
of the short maximum time allowed using RSTTIME1, it does not supply an adequate debounce time for
an external push button circuit. The processor could potentially start running while external components
are still in reset. It is recommended that this signal be used as input only (do not connect to other devices
as a reset) to implement a push button reset circuit to the AM335x, or an output only to be able to reset
other devices after an AM335x reset completes.
http://www.ti.com/lit/ug/spruh73p/spruh73p.pdf