This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 memory map 大小 问题



DSP L2 RAM的大小在手册上说是256K,即地址从0x0080 0000 到0x0083 FFFF。

这里的256K是不是指的地址空间的大小,而不是存储数据量的大小,这里的每个地址是16位,还是32位的。

如果是32位的,L2可以存储的数据量的大小 应该是256*4K字节么?