This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
发的SRIO包里DST ID和 ADDRESS是接收端DSP支持的吗
多谢 已经解决了 谢谢
你好!请问你是怎么解决的啊,我也遇到同样的问题,麻烦给一点指导性建议啊!*_*
我是FPGA和DSP(6672)之间srio通信,FPGA可以收到DSP发的doorbell,但是FPGA发的数据在DDR里完全看不到!搞了好几天了,快崩溃了
如果是DSP6678 ,接不接交换机没啥影响。
1、FPGA给DSP发送的绝对是 DDR3的存储地址,0X80000000;
2、FPGA给DSP发送SRIO必须采用FPGA自带核的组包格式!