This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急!急!关于FPGA通过SRIO发给DSP,直接操作内存空间0X80000000的问题?



自己设计的原理图,2片DSP6678,分别是DSP-A和DSP-B;通过CPS1848(RAPID IO SWITCH)连接,每个DSP 4路SRIO LANE都连上了(初步跑在X4模

式),,FPGA控制DSP和CPS上电、复位。FPGA也和CPS1848连接了。     

软件例程是官网提供的.:目录是\K1_STK_v1.1\K1_STK_v1.1\SRIO 程序是SRIO_Test.c 和 SRIO_2DSP_Test.c

现测试FPGA和DSP之间的通信。通过修改例程,DSP给FPGA发送NWRITE已经成功。

现在问题是,FPGA给DSP发送SRIO数据包,FPGA能显示端口配置正确,FPGA发送数据后,在DSP的内存0X80000000里面没有任何数据?这是为什么啊?

DSP也是通过CPS发过去的,FPGA通过CPS就不行吗?FPGA是用的IP核,自己组数据包,在组包的过程中,SRIO有没有数据大小端的要求?还有,操作的DSP内存地址有没有问题,能不能往这个地址写?多谢,非常着急,多谢了。