This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437X GP EVM 评估板不能Nandflash 启动

Other Parts Discussed in Thread: TPS65218

非常感激上海TI 工程师提供的AM437X GP EVM 评估板,经过几天的摸索和学习,对TI LINUX SDK 有了一些了解,开始做了些实践操作,做了各种尝试,都没法让评估板从NANDFLASH 启动。

我的操作如下:

1)通过SD卡启动(原装SD\自制SD都可以正常引导),控制台信息如下:

U-Boot SPL 2017.01-00360-g87da453-dirty (Nov 25 2017 - 17:43:12)

Trying to boot from MMC1

SPL: Please implement spl_start_uboot() for your board

SPL: Direct Linux boot not active!

reading u-boot.img

reading u-boot.img

reading u-boot.img

reading u-boot.img

U-Boot 2017.01-00360-g87da453-dirty (Nov 25 2017 - 17:43:12 -0800)

CPU  : AM437X-GP rev 1.1

Model: TI AM437x GP EVM

DRAM:  2 GiB

PMIC:  TPS65218

NAND:  512 MiB

MMC:   OMAP SD/MMC: 0

reading uboot.env

** Unable to read "uboot.env" from mmc0:1 **

Using default environment

=> ba dinfo

arch_number = 0x00000000

boot_params = 0x80000100

DRAM bank   = 0x00000000

-> start    = 0x80000000

-> size     = 0x80000000

eth0name    = cpsw

ethaddr     = 34:b1:f7:31:3b:c0

eth1name    = usb_ether

eth1addr    = 34:b1:f7:31:3b:c2

current eth = cpsw

ip_addr     = <NULL>

baudrate    = 115200 bps

TLB addr    = 0xFFFF0000

relocaddr   = 0xFFF2B000

reloc off   = 0x7F72B000

irq_sp      = 0xFDF0FC80

sp start    = 0xFDF0FC70

Early malloc usage: 3a0 / 2000

=> mmcinfo

Device: OMAP SD/MMC

Manufacturer ID: 2

OEM: 544d

Name: SA04G

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 3.6 GiB

Bus Width: 4-bit

Erase Group Size: 512 Bytes

read 1.22 MB/s. error 0/10 (0%)

write ### MB/s. error 0/0 (0%)

=> mtdparts

device nand0 <nand.0>, # parts = 10

 #: name           size           offset                  mask_flags

 0: NAND.SPL            0x00040000 0x00000000     0

 1: NAND.SPL.backup1    0x00040000          0x00040000     0

 2: NAND.SPL.backup2    0x00040000          0x00080000     0

 3: NAND.SPL.backup3    0x00040000          0x000c0000     0

 4: NAND.u-boot-spl-os  0x00080000     0x00100000     0

 5: NAND.u-boot         0x00100000   0x00180000     0

 6: NAND.u-boot-env     0x00040000   0x00280000     0

 7: NAND.u-boot-env.backup10x00040000      0x002c0000     0

 8: NAND.kernel         0x00700000   0x00300000     0

 9: NAND.file-system    0x1f600000      0x00a00000     0

active partition: nand0,0 - (NAND.SPL) 0x00040000 @ 0x00000000

defaults:

mtdids  : nand0=nand.0

mtdparts: mtdparts=nand.0:256k(NAND.SPL),256k(NAND.SPL.backup1),256k(NAND.SPL.backup2

2)通过tftp 下载MLO、u-boot.img 到内存, 在将内存MLO、u-boot.img 写到flash;

tftp 0x82000000 MLO

nand erase 0x0 0x40000

nand write 0x82000000 0x0 0x40000

 

tftp 0x82000000 u-boot.img

nand erase 0x00180000 0x00100000

nand write 0x82000000 0x00180000 0x00100000  \\根据MTD PARTS INFO,写到正确的nandflash 地址

4)   关机,调整SYSBOOT从NANDFALSH 启动;

5)启动后控制台一点信息都没有,说明MLO 都没能正常运行;

6)后来尝试下载各种版本MLO, u-boot.img(SDK Pre build 、原装SD卡、重编U-BOOT ),没有一个能NANDLFLASH 启动。

搜索论坛相关帖,都没有解答,盼TI 工程师给予支持。是否是我的评估板版本太早,ROM 程序或PCB 有缺陷?

 www.deyisupport.com/.../76350.aspx