This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
刚贴装回来的一批新板子,出现了一个现象,就这一块:电源没问题,复位输入和复位输出都没有问题,但是在UART2模式下载ubl和uboot时,一直停在Waiting for BOOTME,我用示波器抓了UART2发送的管脚,按复位时可以检测到UART2管脚发出来的低电平,这种情况说明BOOTME出来了吗?9600和115200的波特率都试过。
能下载的板子硬件和这批一模一样吗?用CCS通过JTAG口看是否能烧写,看是不是uart口的配置问题。
您好:
Shine Zhang ,问题已经找到了,BOOT的上拉电阻选的过大,看来不仅仅是BOTTMODE的01设置问题,还要看BOOT的电压,这块板子是好的,谢谢