This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

自己的硬件上,运行RDK2.8的包应用加载之后,出现网络断链(DM8127)



在我们自己的硬件上,运行RDK2.8的包,当所有的应用加载之后,出现网络断链。
(1)硬件:
网口差异:
我们使用的RMII模式,百兆网口,PHY芯片是DM9161AEP。与Appro相机对比后,我们的网口硬件主要差异在于:我们将PINCNTL232定义成“EMAC_RMREFCLK”功能,而在Appro相机中是作为PHY芯片的中断使用;我们增加了PINCNTL52作为PHY的中断输入;
DDR差异:
我们只使用了一个EMIF0接口,2片256M DDR3内存;
(2)在我们自己的硬件上,之前的RDK1.5包,所有应用加载后,网络正常;RDK3.0包,所有应用加载后,网络断链,现象同RDK2.8;
(3)在我们的硬件上,RDK2.8,RDK3.0如果只加载内核,不加载应用,网络正常;

 在RDK2.8之后的软件包中,是否有应用使用了与网络相关的资源,资源冲突导致断链?
 请帮忙指教,非常感谢!