This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515汇编语句报错



编译之后,Problems显示0 errors,但是未生成.out文件。以上两行代码是例程,有问题吗?还是工程初始设置有问题?

  • 先用asm( " nop " );语句编译试试,看是否是BIT语法的问题。

  • 用asm( " nop " );语句替换以上两行代码编译没有出现问题。以上两行代码进行编译就会报错。而且使用CCS6.1的开发环境,在工程中加入.asm文件,语句也会报错。

  • 我看了一下c55x汇编指令,没有找到BIT指令。

  • 这是官方提供的例程,现在应该如何修改?

  • 请问是哪个例程?

  • #include <stdio.h>
    #include "data_types.h"
    #include "register_system.h"
    #include "register_cpu.h"
    #include "rtc.h"
    #include "control.h"
    #include "i2s.h"
    #include "dma.h"
    #include "timer.h"
    #include "lcd.h"
    #include "sar.h"
    #include "usbstk5515.h"
    #include "usbstk5515_led.h"
    void InitSystem(void);
    void ConfigPort(void);
    void SYS_GlobalIntEnable(void);
    void SYS_GlobalIntDisable(void);
    void BlinkLED(void);
    void GenerateAudioTone(void);
    Uint16 fSineWave = 0;
    Uint16 f1KToneOn =0;
    Uint16 f2KToneOn =0;
    extern Uint16 fTimer;
    extern Uint16 Flag_RTC;
    extern Uint16 Conunt_RTC;
    extern Uint16 halfSecCnt;
    extern void AIC3254_init(void);
    extern Int16 oled_test();
    void main(void)
    {
     Uint16 temp, key, i;
     
       
        InitSystem();
        ConfigPort();
        SYS_GlobalIntEnable();
       
        IER0 = 0x0010;      // enable timer int     
        IER1 = 0x0004;      // enable RTC int
        Timer0Init();
     reset_RTC();
     enable_rtc_second_int();
     AIC3254_init();
     set_i2s0_slave();
        enable_i2s0();
     StartTimer0();
     
     SYS_EXBUSSEL = 0x6100;  // Configure External bus
     oled_test();             // Set display
     USBSTK5515_ULED_init( ); // Configure user LEDs
        Init_SAR();              // Initialize SAR for switches
        USBSTK5515_ULED_setall( 0x00 );
       
        while(1)
        {
      //*(ioport volatile unsigned *)0x0001 = 0x03FF;
      //asm(" idle");
            BlinkLED();
      GenerateAudioTone();
    #if 1  
      for ( i = 0 ; i < 4 ; i++ )
            {
                USBSTK5515_ULED_on( i );       // Turn on user LED i
                USBSTK5515_waitusec( 50000 );
            }
            for ( i = 0 ; i < 4 ; i++ )
            {
                USBSTK5515_ULED_off( i ); // Turn off user LED i
                USBSTK5515_waitusec( 50000 );
            }
    #else
      /* Get Switch values an toggle LEDs accordingly */
         key = Get_Sar_Key();
         if((key == SW1))   // If SW1 pressed
         {
          USBSTK5515_ULED_toggle( 0 );  // Toggle DS2 (GREEN LED)
         }
         if((key == SW2))   // If SW2 pressed
         {
          USBSTK5515_ULED_toggle( 3 );  // Toggle DS5 (BLUE LED)
         }
         if((key == SW12))   // If SW1 and SW2 pressed
         {
          USBSTK5515_ULED_toggle( 1 );  // Toggle DS3 (RED LED)
          USBSTK5515_ULED_toggle( 2 );  // Toggle DS4 (YELLOW LED)
         }
    #endif
     }
    }
    void InitSystem(void)
    {
     Uint16 i;
    // PLL set up from RTC
        // bypass PLL
        CONFIG_MSW = 0x0;
    #if (PLL_100M ==1)
        PLL_CNTL2 = 0x8000;
        PLL_CNTL4 = 0x0000;
        PLL_CNTL3 = 0x0806;
        PLL_CNTL1 = 0x82FA;
       
    #elif (PLL_12M ==1)
        PLL_CNTL2 = 0x8000;
        PLL_CNTL4 = 0x0200;
        PLL_CNTL3 = 0x0806;
        PLL_CNTL1 = 0x82ED;
    #elif (PLL_98M ==1)   
     // 98.304 MHz
        PLL_CNTL2 = 0x8000;
        PLL_CNTL4 = 0x0000;
        PLL_CNTL3 = 0x0806;
        PLL_CNTL1 = 0x82ED;
       
    #endif
        while ( (PLL_CNTL3 & 0x0008) == 0);
        // Switch to PLL clk
        CONFIG_MSW = 0x1;
    // clock gating
    // enable all clocks
        IDLE_PCGCR = 0;
        IDLE_PCGCR_MSW = 0xFF84;
       
    // reset peripherals
        PER_RSTCOUNT = 0x02;
        PER_RESET = 0x00fb;   
        for (i=0; i< 200; i++);
       
    }
    void ConfigPort(void)
    {
        //  configure ports
        PERIPHSEL0 = 0x6900;        // parallel port: mode 6, serial port1: mode 2, serial port0: mode1
       
    }

    void SYS_GlobalIntEnable(void)
    {
        asm(" BIT (ST1, #ST1_INTM) = #0");
    }
    void SYS_GlobalIntDisable(void)
    {
        asm(" BIT (ST1, #ST1_INTM) = #1");
    }

    static toggleLED(void)
    {
     Uint16 temp;
        temp = ST1_55;
        if((temp&0x2000) == 0)
        {
            // turn on LED
            temp |= 0x2000;
        }
        else
        {
            // turn off LED
            temp &=0xDFFF;
        }
        ST1_55 = temp;
    }

    void BlinkLED(void)
    {
    #if 1
     if(fSineWave==1)
     {
         if(Flag_RTC ==1)
      {
            Flag_RTC =0;
       toggleLED();
      }
     
     }
     else
     {
         if(fTimer ==1)
      {
            fTimer =0;
       toggleLED();
      }
     }

    #else
        if(Flag_RTC ==1)
     {
          Flag_RTC =0;
      toggleLED();
     }
    #endif
    }
    void GenerateAudioTone(void)
    {
     if(Conunt_RTC < 10)
     {
      if(f1KToneOn ==1)
       return;
      // 1KHz sine wave
      fSineWave = 1;
      f1KToneOn =1;
      f2KToneOn =0;
            set_dma0_ch0_stop();
         set_dma0_ch1_stop();
            set_dma0_ch0_i2s0_Lout();
         set_dma0_ch1_i2s0_Rout();
     }
     else if (Conunt_RTC < 20)
     {
      if(f2KToneOn ==1)
       return;
      // 2KHz sine wave
      fSineWave = 0;
      f1KToneOn =0;
      f2KToneOn =1;
            set_dma0_ch0_stop();
         set_dma0_ch1_stop();
            set_dma0_ch0_i2s0_Lout();
         set_dma0_ch1_i2s0_Rout();
     }
     else
     {
      Conunt_RTC =0;
      f1KToneOn =0;
      f2KToneOn =1;
     }
    }
    以上例程。并且加入vector.asm,涉及中断的文件就会报错。
  • BIT属于algebraic指令,试试到Properties -> C/C++-Build -> Runtime Model Options下面,把--algebraic,-mg选项勾一下。

  • 这样改变之后,又会出现其它问题。以上语句不属于algebraic,编译无法通过。

  • 可以右击含BIT语句的那个文件属性,单独对该文件设置-mg选项,这样不会影响其它文件。

  • 非常非常感谢您的帮助!!!!!