This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127在引导内核中卡住的问题2



你好:

        我使用的芯片是DM8127,是自己做的的板子,原理图见附件《DM8127原理图.pdf》。购买的开发板是广州创龙公司的DM8148开发板(软件开发包是广州创龙从TI8148开发板的开发包上改的)。

        由于我自己板子的DM8127只使用了DDR0接口,没有使用DDR1,所以我修改了u-boot\arch\arm\include\asm\arch-ti81xx\ddr_def_ti814x.h文件,具体修改内容如下:

  1. 第300行,#define DDR3_EMIF_SDRAM_CONFIG  0x61C11B32 改为:

                             #define DDR3_EMIF_SDRAM_CONFIG  0x61C11A32 //RowAddress A0-A13

       2.  第321行,#define PG2_1_DMM_LISA_MAP_3  0x80740300 改为:

                            #define PG2_1_DMM_LISA_MAP_3  0x80700300 //No interleaving模式

       然后重新编译u-boot,生成新的MLO和u-boot.bin,替换了开发板原配SD卡中的对应文件。

       将这张SD卡插到我的板子后,上电,串口终端在booting the kernel后卡住不动了,如下图所示:

  

   经过在内核start_kernel函数中添加打印信息,发现在调用schedule()函数后就卡住了,请问能帮我分析一下问题可能出在哪里吗?

  我这个SD卡插在创龙开发板上是可以正常启动的。