This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5517的烧录问题



 你好,

            C5517有多少种烧录方式? 我们设计了一款产品使用MTK手机方案做4G网络配置,搭配C5517做语音处理方案。需要有在线更新DSP软件的功能,请问应该如何实现,软硬件如何设计?谢谢!

  • 那只能用UART了,注意要4线模式。

    C5517片上内存够吗?要扩内存吗?也可以看看C5545,小一点。

  • 4线模式是指UART_CTS,ART_RTS,UART_TXD,UART_RXD这四路接我们控制端的两路uart吗?这样会占用一组i2s接口,是否可以共用线路?

    调试阶段可以使用仿真器通过USB烧录?

     

     C5517是TI推荐的,现在是在实际项目中调试我们的算法,所以也需用了性能稍微强大一些的C5517。谢谢!

  • uart和i2s是管脚复用的,在uart boot完成后,主程序里修改EBSR寄存器来使能I2S接口。

    直接通过仿真器运行烧写程序即可,见下面的wiki网站。

    http://processors.wiki.ti.com/index.php/C5517_Boot-Image_Programmer