I am developing on L138 platform, debug DSP core now.
Software env: ccs6.10
Sysbios:6.34.4.22
XDCTools:3.24.5.48
I downloaded the UIA1.2.0.7 component from the official website according to the version information of Sysbios and XDCTools.
According to UIA instructions for the configuration, than in the simulation environment select Tools - >RTOS Analysis - > Load Analysis, in the pop-up window, Instrumentation status display “cannot determine”, if next step, subsequent Analysis window without any data.
Is it a version issue, or is the UIA configuration incorrect or the simulation environment set up incorrect?