出现如下形式提示,请问是什么问题?用的OMAPL138芯片
ARM9_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01C11138 at (*((unsigned int *) (0x01C11000+0x138))|=0x1) [omapl138.gel:25] at device_PLL0(0, 18, 0, 0, 1, 3, 9) [omapl138.gel:426] at Set_Core_456MHz() [omapl138.gel:443] at Core_456MHz_DDR2_156MHz() [omapl138.gel:261] at CPU_PLL_PSC_DDR_Init() [omapl138.gel:251] at OnTargetConnect() .
ICEPICK_C: Power Failure on Target CPU
ICEPICK_C: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
ARM9_0: Error: Failed to get PRSC status
ARM9_0: Unable to determine target status after 20 attempts
ARM9_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging