SRIO配置成4个port,每个port 是1个lane,且连接了4个设备,现在通过维护包来访问DSP的id ,虽然是4个不同的设备连接到了不同的port,但是在交换机网络中,维护包扫描到的DSP的ID是一样的。
手册表明,base_id0-15,其中1-15和BBR寄存器有关。
问题:
1:维护包扫描到的只是base_id 1??不管是通过那个端口吗??
2:怎么实现 1个端口和一个ID绑定,不是指在传输层通过BRR来判断数据的接受,想知道维护包实现不同端口,不同的ID??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没太明白您的意思,您是说SWITCH的4个PORT 都是链到4个器件(其中1个是DSP),还是说TI DSP的4 个PORT链接到外面srio device上?