This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5509A并行flash上电无法自举,请教调试思路。



5509A采用EMIF外接16位flash并行自举失败。

1、我在同一块pcb上设计了两个一样的dsp系统,一个通道上电自举成功,另一个通道相同的程序上电无法自举;

2、程序已正确烧录到flash;

3、两通道均可连接仿真器在线调试;

4、GPIO0-3按照datasheet要求设置为1110,在dsp引脚上测试电平正常;

5、上电或复位时,正常通道的ce1引脚有短暂的周期性低电平使能信号,无法自举通道ce1一直为高电平(两通道的ce1信号在在线调试时均正常);

6、测过地址A1的信号,上电时,正常通道有数据输出,无法自举通道无数据输出。

请问大家,是不是芯片有问题,下一步应该怎样调试?