This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 对晶振频率稳定度指标要求

Other Parts Discussed in Thread: OMAP-L138

OMAPL138如果采用25MHz晶振作为外部时钟输入的话,对晶振的频率稳定度指标有什么要求?

  • 在数据手册上有说明。
    For input clockfrequencies between 20 and 30 MHz, a crystal with 60 ohm max ESR is recommended. Typical load capacitance values are 10-20 pF, where the load capacitance is the series combination of C1 and C2.

    6.5 Crystal Oscillator or External Clock Input
    http://www.ti.com/lit/ds/symlink/omap-l138.pdf