我下载了am335x的linux SDK.linux启动之后,看到启动了matrix gui.我想自己修改matrix gui,不知道哪里可以下载到这个应用的源码,
我有访问http://processors.wiki.ti.com/index.php/Matrix_Users_Guide,但是上面的gforge网站不允许下载.
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我下载了am335x的linux SDK.linux启动之后,看到启动了matrix gui.我想自己修改matrix gui,不知道哪里可以下载到这个应用的源码,
我有访问http://processors.wiki.ti.com/index.php/Matrix_Users_Guide,但是上面的gforge网站不允许下载.
谢谢!
试试git clone git://git.ti.com/matrix-gui-v2/matrix-gui-v2.git
git clone git://git.ti.com/matrix-gui-v2/matrix_browser.git
git clone git://git.ti.com/matrix-gui-v2/matrix-gui-v2-apps.git
您好,我编译sdk出现这样的错误,我单独编译u-boot和linux就没有事,但是编译matrix-gui,arm-benchmarks那些就有会发生如图所示的错误。能帮我解决一下吗?
Building ARM Benchmarks
=============================
make[1]: Entering directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3'
for dir in dhrystone whetstone linpack; do \
make -C $dir debug; \
done
make[2]: Entering directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3/dhrystone'
/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-gcc -g3 -gdwarf-2 -DTIME -c -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard -oDebug/dhry_1.o dhry_1.c
In file included from dhry_1.c:56:0:
dhry.h:432:19: fatal error: stdio.h: No such file or directory
#include <stdio.h>
^
compilation terminated.
make[2]: *** [Debug/dhry_1.o] Error 1
make[2]: Leaving directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3/dhrystone'
make[2]: Entering directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3/whetstone'
/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-gcc -g3 -gdwarf-2 -fmessage-length=0 -Wall -c -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard -oDebug/whetstone.o whetstone.c
whetstone.c:93:20: fatal error: stdlib.h: No such file or directory
#include <stdlib.h>
^
compilation terminated.
make[2]: *** [Debug/whetstone.o] Error 1
make[2]: Leaving directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3/whetstone'
make[2]: Entering directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3/linpack'
/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-gcc -g3 -gdwarf-2 -DUNROLL -DSP -fmessage-length=0 -c -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard -oDebug/linpack.o linpack.c
linpack.c:89:19: fatal error: stdio.h: No such file or directory
#include <stdio.h>
^
compilation terminated.
make[2]: *** [Debug/linpack.o] Error 1
make[2]: Leaving directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3/linpack'
make[1]: *** [debug] Error 2
make[1]: Leaving directory `/home/goembed/ti-processor-sdk-linux-am335x-evm-04.03.00.05/example-applications/arm-benchmarks-1.3'
make: *** [arm-benchmarks] Error 2