This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
调试6678过程中,给两个核烧写程序,烧完出现如下错误:Error connecting to the target(Error - 1143 @0x0)C66xx_0: Error connecting to the target: (Error -1143 @ 0x0) Device core was hung. The debugger has forced the device to a ready state and recovered debug control, but your application's state is now corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further。
后来仿真器可以连上,debug进不去,断电上电也不行,reset也不行。求大神支招,急!!!
emif接的是flash吗? 如果是烧写完emif flash后出现这个问题,可能是flash里的代码跑飞影响仿真器的连接。
用镊子将CS与3.3V短接再上电,然后断开镊子去连仿真器,再跑程序将flash擦掉。或者更改boot mode。