本人最近在配置ths8200的nVGA输出,遇到了一些问题,向各位请教
1, Ths8200的配置文件。VGA配置第一行说明
DATASET_NAME,"THS8200_SXGA60Hz-108MHz ( 20 bit 4:2:2, embedded) HS/VSout +/+, YCbCr>RGB"
这个108Mhz是指ths8200的CLKIN要为108Mhz么,还是其它?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人最近在配置ths8200的nVGA输出,遇到了一些问题,向各位请教
1, Ths8200的配置文件。VGA配置第一行说明
DATASET_NAME,"THS8200_SXGA60Hz-108MHz ( 20 bit 4:2:2, embedded) HS/VSout +/+, YCbCr>RGB"
这个108Mhz是指ths8200的CLKIN要为108Mhz么,还是其它?
1. shide
2.我这网络看不到图
3. 是的。你可以设置color bar寄存器直接看图像的
十分感谢eason wang的回答
第二个问题很关键
其实是关于dm6467的VPIF时钟,主要是指VPIF_CLKIN3与VPIF_CLKOUT2,VPIF_CLKIN3是要接外部时钟,我接的是74.25M的晶振。VPIF_CLKOUT2是输出时钟,提供给THS8200,请问这个时钟能够通过寄存器进行配置么,如何在内核里面对它的大小进行配置?
我再将图贴上去
2, VPIF与ths8200的连接如下(板子自己设计的,没有用cde,固定晶振74.25M):

这个问题,在查阅了TI的手册,可是一直没有找到答案。。。。。。
你好,我最近也在弄THS8200芯片,但是DM6467输出的是16位的BT1120格式的图像数据,不知道怎么连到VGA输出,你能把原理图发个给我吗,谢谢了,1449485095@qq.com。