This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am437x 外接spi flash设备 spi4引脚无任何波形输出,初始化是按照正常的方法执行的,不知道哪里有问题,求教



1 首先我在设备树中初始化了spi4的引脚
    spi4_default: pinmux_spi4_default {
        pinctrl-single,pins = <
            0x250 (PIN_OUTPUT_PULLDOWN    |         MUX_MODE0)    /* spi4_clk.spi0_clk */
            0x254 (PIN_INPUT     |         MUX_MODE0)    /* spi4_d0.spi0_d0 */
            0x258 (PIN_OUTPUT    |         MUX_MODE0)        /* spi4_d1.spi0_d1 */
            0x230 (PIN_OUTPUT_PULLDOWN  | MUX_MODE2)        /* spi4_cs1*/
        >;
    };

2 让后使能spi4

&spi4 {
    pinctrl-names = "default";
    pinctrl-0 = <&spi4_default>;
    status = "okay";
};

3 在driver/spi/目录下添加了spi_board_info结构体

     {
         .modalias = "w25q16",  /* 对应的spi_driver名字也是"w25q16" */
         .max_speed_hz = 10000000,    /* max spi clock (SCK) speed in HZ */
         .bus_num = 1,     /* 接在SPI CONTROLLER 1 */
         .mode    = SPI_MODE_0,
         .chip_select   = 0, /* flash_cs, 它的含义由spi_master确定 */
     }

4 加载上驱动程序可以进入probe函数,就是无法读取设备ID号,通过逻辑分析仪抓取不到任何spi4的波形,

我是不是哪里漏操作了步骤,第一次用ti的开发板,请大神指导!