导入3.3工程,然后编译,为啥报错?
Buildfile generation error occurred..
This project's device is not supported by compiler version 8.2.2:
- See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if required compiler is available through a CCS update.
- Visit CCS App Center to get the latest compiler support.
- Or download and install the required compiler [http://software-dl.ti.com/codegen/non-esd/downloads], then register it with CCS through 'Preferences > CCS > Build > Compilers'.
Build stopped..
Description Resource Path Location Type
This project's device is not supported by compiler version 8.2.2. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if required compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the required compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. NANDWriter_DSP properties Problems